Features of 4th Gen EPD Controller in i.MX7?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Features of 4th Gen EPD Controller in i.MX7?

1,063件の閲覧回数
teazia
Contributor I

I would like to know the features of the 4th Generation EPD controller in the i.MX7 as opposed to earlier generations.  Is this generation of features also avialble in a discrete Controller that is not an embedded on a SOC?

Thank you!

ラベル(2)
0 件の賞賛
返信
1 返信

953件の閲覧回数
art
NXP Employee
NXP Employee

For the detailed description of the i.MX7Dual EPD Controller feature set, please refer to the Section 13.6 of the i.MX7Dual Reference Manual document, available on the processor's Documentation web page:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

NXP does not provide a discrete EPD Controller solution.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信