I tried update image by fastboot on IMX6 custom board (refer to sabresd board), but something was wrong at first step,
I can't connect to device and error message as following:
MX6Q SABRESD U-Boot > fastboot | |
fastboot is in init......flash target is MMC:2 |
wait usb cable into the connector!
Correct me if I'm wrong,
I think the pin definition should be modified,
but I don't know which pin?
Thank you!
Hi Public Account
had you attached USB cable between host PC and i.MX6 USB OTG,
as describes attached document sect.8.2 How do I use Android fastboot?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------