Fast path Data processing on i.MX6Q ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fast path Data processing on i.MX6Q ?

1,122 次查看
yogeshgupta
Contributor I

Hi All

We are using Freescale i.MX6Q Soc in our product as a control processor and want to process some specific type of traffic on fast path.

As this SOC is a Quard core so can I run linux kernel on 3 cores and Simple executable(Run to completion) on 4th Core for my fast path data processing.

Any one tried such type of scheme in any of iMX6 product?

Also can I fetch a specific type of network packet directly without traversing Ethernet driver and IP stack on core without LINUX.

Please suggest some workaround if it is not possible.

Thanks in advance

Y Gupta

0 项奖励
回复
1 回复

950 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yogesh

one can implement  this following three steps :

1. Add the parameter isolcpus=[cpu_number] to the Linux kernel command line form the boot loader during

boot. This will instruct the Linux scheduler to no run any regular tasks on that CPU unless specifically

requested using cpu affinity.

2. Use CPU affinity to fix your specific task to the isolated CPU.

3. Use IRQ affinity to set other CPUs to handle all interrupts so that your isolated CPU will not receive any

interrupt. Some useful references:

https://community.freescale.com/thread/301130

https://community.freescale.com/message/604888#604888

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复