Fast enternet PHY of i.MX53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fast enternet PHY of i.MX53

1,088件の閲覧回数
chunlinchen
Contributor I

hi,everyone:

   I have a i.MX53QSB,the NO. is 700-27104 REV C.Now ,I have a question,when i plug the enternet cable ,the PC does not connect my i.MX53QSB.shall i input the new IP for i.MX53,and anybody knows the IP?

          best  regards!

ラベル(4)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

970件の閲覧回数
BrilliantovKiri
Senior Contributor I

Hello!

If I right, QSB use DHCP by default, you can configure it manualy after system boot or change U-Boot configuration.

0 件の賞賛
返信

970件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

I agree, you need to have a router to give an IP address to the board. Since by default the QSB it is configure with DCHP mode.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信