Fast enternet PHY of i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fast enternet PHY of i.MX53

803 Views
chunlinchen
Contributor I

hi,everyone:

   I have a i.MX53QSB,the NO. is 700-27104 REV C.Now ,I have a question,when i plug the enternet cable ,the PC does not connect my i.MX53QSB.shall i input the new IP for i.MX53,and anybody knows the IP?

          best  regards!

Labels (4)
0 Kudos
Reply
2 Replies

685 Views
BrilliantovKiri
Senior Contributor I

Hello!

If I right, QSB use DHCP by default, you can configure it manualy after system boot or change U-Boot configuration.

0 Kudos
Reply

685 Views
jamesbone
NXP TechSupport
NXP TechSupport

I agree, you need to have a router to give an IP address to the board. Since by default the QSB it is configure with DCHP mode.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply