Failure to prepare SD card with prebuilt Linux image through MFG tool in Win 7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failure to prepare SD card with prebuilt Linux image through MFG tool in Win 7

1,654 Views
aye_thida
Contributor I

Hi All

 

Regarding porting prebuilt image into SD card installed in our i.mx6Q platform , I have encountered the following issue.

When Linux prebuilt image is put into SD card , the attached error has come out and then need to stop the operation unsuccessfully. 

 

Target Sabre board P/N : MCIMX6Q-SDP

Host PC OS : Win 7

Linux BSP used(Prebuilt Image) : L3.14.52_1.1.0-ga_images_MX6QDLSOLO.tar

MFG tool used : L3.14.52_1.1.0_ga-mfg-tools.tar

SW6 DIP switch setting : 00001100

 

Attached are “Error” , HyperTerminal screen shoot and MFG log file.

 

Appreciated if anyone help to figure out on the issue.

 

Best Regards

Aye

Original Attachment has been moved to: MfgTool-Log.txt.zip

0 Kudos
Reply
1 Reply

1,532 Views
Yuri
NXP Employee
NXP Employee

Hello,

The simplest way to test the system, using demo images is to copy
image to SD card, as described in section 4.3.2 (Copying the full SD

card image) of “i.MX_Linux_User's_Guide.pdf”

http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS

The SD demo images are as following :

fsl-image-gui-x11-imx6qdlsolo.rootfs.sdcard

fsl-image-qt5-x11-imx6qdlsolo.rootfs.sdcard

Please try it first.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply