Failing to playback the image with gst-launch-1.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Failing to playback the image with gst-launch-1.0

588 次查看
Kenji-EU-NEC
Contributor I

Reference: Uploaded log file.

 

Setup/Preconditions:

Platform based on i.MX8M-Plus.

Yocto kernel version: 5.15.32 (Yocto 4.0, Kirkstone)

HDMI cable for display. Confirmed GUI of Yocto is displayed on the screen

 

Process:

As seen in the uploaded log file,,, after loading the taget jpg file saved in USB, run the below,

gst-launch-1.0 -v filesrc location=/media/usb/Paris-Image.jpg  ! waylandsink

 

Expectation: Displays its jpg file on the screen (HDMI)

Output: Failure as shown in log file

 

Question(s):

I believe (cannot remember), I built the image with imx-image-core which should be OK to do it. For just in case, I have actually done with other image name,,,, is there any image name that gst-launch-1.0 with wayland would not work (i.e. core-image-minimal)?

Any other suggestions what I should check?

 

 

标签 (1)
0 项奖励
回复
1 回复

556 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Kenji-EU-NEC 

 

I hope you are doing well.

 

You can check the Yocto project user's guide in table Table 1. i.MX Yocto project images:

Alejandro_Salas_0-1724105540490.png

 

Also, you can refer to the Images Yocto documentation.

 

Best regards,

--... ...--

Salas.

0 项奖励
回复