Failed to use MfgTool for i.MX6 with Yocto Project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Failed to use MfgTool for i.MX6 with Yocto Project

1,378 次查看
yuhuiliu1
Contributor I

We want to upgrade from i.MX6 DualLite to i.MX6 QuadPlus.

In i.MX6DL, we used i.MX Yocto Project BSP with imx-4.1.15-2.1.0.

In i.MX6QP, we also used the same setting.

We built image in the following commands:

$ DISTRO=fsl-imx-wayland MACHINE=imx6qpsabresd source fsl-setup-release.sh -b build-image

$ bitbake fsl-image-qt5-validation-imx

Then flashing image to sdcard:

        $ sudo dd if=fsl-image-qt5-validation-imx-imx6qpsabresd-20191209095719.rootfs.sdcard of=/dev/sdb bs=1M conv=fsync

We used this sdcard on i.MX6QP but didn’t work. (nothing happened on i.MX6QP)

We used another way – MfgTool but stock at loading U-boot for a long time.

标签 (3)
0 项奖励
回复
2 回复数

1,267 次查看
radhikasomaiya
Senior Contributor II

Hi yuhuiliu@luxvisions-inno.com ,

We are able to build  L4.1.15-2.1.0 image for  i.MX 6QuadPlus Sabre board and boot i.MX 6QuadPlus Sabre board using L4.1.15-2.1.0 sdcard image. So can you please try to compile u-boot image and try to boot board using only u-boot image. make sure that your boot mode switches are correct to boot from sd card.

Regards,

Radhika Somaiya.

0 项奖励
回复

1,267 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,


It seems that the image is missing uboot, please try by copying the bootloader directly to your SD

$ sudo dd if=<u-boot image> of=/dev/sdx bs=512 seek=2 conv=fsync

 

Hope this helps,

Regards,

Aldo.

0 项奖励
回复