Failed to mount mmcblk2p4 block

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to mount mmcblk2p4 block

2,112 Views
hominjeon
Contributor I

The mount fails during boot.

EXT4-fs (mmcblk2p5): mounted filesystem with ordered data mode. Opts: (null)
EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option
EXT4-fs warning (device mmcblk2p4): ext4_clear_journal_err:4497: Filesystem error recorded from previous mount: IO failure
EXT4-fs warning (device mmcblk2p4): ext4_clear_journal_err:4498: Marking fs in need of filesystem check.
EXT4-fs (mmcblk2p4): warning: mounting fs with errors, running e2fsck is recommended
EXT4-fs (mmcblk2p4): recovery complete
EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
EXT4-fs (mmcblk2p6): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p6): recovery complete
EXT4-fs (mmcblk2p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)
EXT4-fs (mmcblk2p9): recovery complete
EXT4-fs (mmcblk2p9): mounted filesystem with ordered data mode. Opts: (null)
init: /dev/hw_random not found

I want to know why it fails.

Labels (1)
0 Kudos
4 Replies

1,352 Views
hominjeon
Contributor I

Thank you for your answer.
Your answer was helpful to me.

0 Kudos

1,352 Views
hominjeon
Contributor I

This mmc is KLM8G1GEND-B031 by samsung.

I formated it. and It running normally after formatting.

but, I want to know why the filesystem is damaged.

0 Kudos

1,352 Views
jimmychan
NXP TechSupport
NXP TechSupport

Sometime the filesystem may be corrupted when power lose suddenly.

1,352 Views
jimmychan
NXP TechSupport
NXP TechSupport

what is this mmc device? have you try to format it ?  the filesystem may be damaged so you cannot mount it.

0 Kudos