Hello,
I am running Linux-3.0.35-4.0.0 from freescale on i.MX6 SABRE-AI board.
When I run startx, I get following error.
(II) LoadModule: "vivante"
[ 4915.038] (II) Loading /usr/lib/xorg/modules/drivers/vivante_drv.so
[ 4915.040] (EE) Failed to load /usr/lib/xorg/modules/drivers/vivante_drv.so: /usr/lib/xorg/modules/drivers/vivante_drv.so: cannot open
[ 4915.040] (II) UnloadModule: "vivante"
[ 4915.040] (II) Unloading vivante
[ 4915.040] (EE) Failed to load module "vivante" (loader failed, 7)
[ 4915.040] (EE) No drivers available.
I have compiled kernel and rootfs using LTIB and copied vivante_drv.so (hence generated) to /usr/lib/xorg/modules/drivers folder in the filesystem.
My doubt is that vivante_drv.so file is not matching the kernel version(linux-3.0.35-4.0.0) or xorg driver version(in my case X.Org Video Driver: 13.0).
How do identify what is happening exactly??
Also, can you point me to the repository from where I can download the libraries compiled for the above mentioned version of xorg and Linux combination?
Regards,
Prathamesh
Hello, guys,
Is there any resolutions?
Thanks