Failed to fetch the package from git://git.freescale.com/imx/linux-2.6-imx.git

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to fetch the package from git://git.freescale.com/imx/linux-2.6-imx.git

ソリューションへジャンプ
2,473件の閲覧回数
xjli
Contributor II

I am trying to build yocto project for i.mx6 board on Ubuntu 14.04

when running the commands "repo init " and "repo sync", it always failed, so the relative packages were downloaded from the webpage according to the xml file.

And then when running the command "bitbake fsl-image-qt5", there existed an error that failed to fetch the package from git://git.freescale.com/imx/linux-2.6-imx.git.

I tried to run the command "git clone git://git.freescale.com/imx/linux-2.6-imx.git" in the shell, it always appeared that connection timed out. however, I can access this address by the webpage. I can't resolve it, so I need help. Thank you.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,891件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Perhaps the problem concerns with proxy configuration (if used in Your case).

Unable to obtain/git manifest fsl-arm-yocto-bsp.git, 'connection timed out' 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,892件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Perhaps the problem concerns with proxy configuration (if used in Your case).

Unable to obtain/git manifest fsl-arm-yocto-bsp.git, 'connection timed out' 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信