Hi all,
I'm new to yocto build and I'm having a build problem here. Please help me.
| checking for getauxval... yes
| checking for libseccomp... (cached) no
| checking for libcrypto... no
| checking for librt... yes
| checking how to link with librt... -lrt
| checking for pthread_mutex_lock... yes
| checking for library containing u8_normalize... no
| configure: error:
| ***
| *** Libunistring was not found. To use the included one, use --with-included-unistring
|
| WARNING: exit code 1 from a shell command.
|
ERROR: Task (/home/yoctobuildmachine/Desktop/Yocto/imx-yocto-bsp/sources/poky/meta/recipes-support/gnutls/gnutls_3.6.13.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 576 tasks of which 575 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/yoctobuildmachine/Desktop/Yocto/imx-yocto-bsp/sources/poky/meta/recipes-support/gnutls/gnutls_3.6.13.bb:do_configure
Summary: There were 2 ERROR messages shown, returning a non-zero exit code