Failed to Build imx-image-full with git-native compile error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Failed to Build imx-image-full with git-native compile error

跳至解决方案
3,725 次查看
timorkal
Contributor I

I am trying to build imx-image-full on Ubuntu 24.04 LTS server.

I am using the latest versions for all the packages and the imx8

Command line:
repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.52-2.2.0.xml
DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup release.sh -b build
bitbake imx-image-full

Error:
WARNING: Host distribution "ubuntu-24.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |#########################################################################################################################################| Time: 0:00:05
Loaded 5730 entries from dependency cache.
Parsing recipes: 100% |#######################################################################################################################################| Time: 0:00:01
Parsing of 3654 .bb files complete (3653 cached, 1 parsed). 5731 targets, 377 skipped, 3 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "2.8.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mp-lpddr4-evk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "6.6-scarthgap"
TUNE_FEATURES = "aarch64 armv8a crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:200d12b6a58ad961d60a7774ca0f7a9d29498724"
meta-oe
meta-multimedia
meta-python = "HEAD:72018ca1b1a471226917e8246e8bbf9a374ccf97"
meta-freescale = "HEAD:0627128b341cfb2bef7a0832ce8cac0ce1127f13"
meta-freescale-3rdparty = "HEAD:6c063450d464eb2f380443c7d9af1b94ce9b9d75"
meta-freescale-distro = "HEAD:b9d6a5d9931922558046d230c1f5f4ef6ee72345"
meta-imx-bsp
meta-imx-sdk
meta-imx-ml
meta-imx-v2x = "HEAD:219f6d04a4c339eb6f2dc626f944bbdf9a716ff5"
meta-nxp-demo-experience = "HEAD:e8e646e22b1f926aac83bb7ad522efa9cd8ccc45"
meta-nxp-matter-baseline
meta-nxp-openthread = "HEAD:f58365ec75a5768ff3e8e8bcd64f237738c93160"
meta-arm
meta-arm-toolchain = "HEAD:950a4afce46a359def2958bd9ae33fc08ff9bb0d"
meta-clang = "HEAD:2b7433611d80f6d0ee1b04156fa91fc73d3c2665"
meta-gnome
meta-networking
meta-filesystems = "HEAD:72018ca1b1a471226917e8246e8bbf9a374ccf97"
meta-qt6 = "HEAD:586a6cb5aec755803a3be3cec359baafe89d6432"
meta-parsec
meta-tpm = "HEAD:459d837338ca230254baa2994f870bf6eb9d0139"
meta-virtualization = "HEAD:6f3c1d8f90947408a6587be222fec575a1ca5195"

Sstate summary: Wanted 5228 Local 0 Mirrors 0 Missed 5228 Current 2596 (0% match, 33% complete)################################################# | ETA: 0:00:01
Initialising tasks: 100% |####################################################################################################################################| Time: 0:00:15
NOTE: Executing Tasks
ERROR: git-native-2.44.1-r0 do_compile: oe_runmake failed
ERROR: git-native-2.44.1-r0 do_compile: ExecutionError('/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/temp/run.do_compile.60384', 1, None, None)
ERROR: Logfile of failure stored in: /mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/temp/log.do_compile.60384
Log data follows:
| DEBUG: Executing python function autotools_aclocals
| DEBUG: SITE files ['endian-little', 'common-linux', 'common-glibc', 'bit-64', 'x86_64-linux', 'common']
| DEBUG: Python function autotools_aclocals finished
| DEBUG: Executing shell function do_compile
| NOTE: make -j 16 NO_PYTHON=1 CFLAGS=-isystem/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/include -O2 -pipe LDFLAGS=-L/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib -L/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib -Wl,-rpath,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib -Wl,-rpath,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 -pthread PERL_PATH=/usr/bin/env perl COMPUTE_HEADER_DEPENDENCIES=no NO_GETTEXT=1 NO_CROSS_DIRECTORY_HARDLINKS=1
| LINK git
| LINK scalar
| /mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/hosttools/ld: common-main.o: in function `main':
| common-main.c:(.text.startup+0xde): undefined reference to `cmd_main'
| collect2: error: ld returned 1 exit status
| make: *** [Makefile:2833: scalar] Error 1
| make: *** Waiting for unfinished jobs....
| /mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/hosttools/ld: git.o:(.data.rel+0x7d0): undefined reference to `cmd_pack_objects'
| /mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/hosttools/ld: git.o:(.data.rel+0xb60): undefined reference to `cmd_submodule__helper'
| /mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/hosttools/ld: git.o:(.data.rel+0xd10): undefined reference to `cmd_worktree'
| collect2: error: ld returned 1 exit status
| make: *** [Makefile:2418: git] Error 1
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (virtual:native:/mnt/disks/yocto_disk/imx-yocto-bsp/sources/poky/meta/recipes-devtools/git/git_2.44.1.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2220 tasks of which 2216 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
virtual:native:/mnt/disks/yocto_disk/imx-yocto-bsp/sources/poky/meta/recipes-devtools/git/git_2.44.1.bb:do_compile
Summary: There was 1 WARNING message.
Summary: There were 2 ERROR messages, returning a non-zero exit code.

0 项奖励
回复
1 解答
3,629 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please go to folder "imx-yocto-bsp_scarthgap/build/tmp/work/x86_64-linux/git-native/2.44.1/git-2.44.1" and check whether you could run the following commands sucessfully.

$ make distclean

$ make -j 4 NO_PYTHON=1 CFLAGS='-isystem/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/include -O2 -pipe' LDFLAGS='-L/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib -L/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib -Wl,-rpath,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib -Wl,-rpath,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 -pthread' PERL_PATH='/usr/bin/env perl' COMPUTE_HEADER_DEPENDENCIES=no NO_GETTEXT=1 NO_CROSS_DIRECTORY_HARDLINKS=1

 

在原帖中查看解决方案

0 项奖励
回复
9 回复数
3,538 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please go to folder build/tmp/work/x86_64-linux/git-native/2.44.1/git-2.44.1/

run the following command.

$ make distclean

Then add the following line in build/conf/local.conf.

PARALLEL_MAKE ?= "-j 4"

Then run 

$ bitbake imx-image-full

0 项奖励
回复
3,694 次查看
yipingwang
NXP TechSupport
NXP TechSupport

In OpenEmbedded-Core, :term:`ASSUME_PROVIDED`  mostly specifies native
tools that should not be built. An example is ``git-native``, which
when specified, allows for the Git binary from the host to be used
rather than building ``git-native``.

 

Please install the following package on your host PC.

$ sudo apt install gawk wget git diffstat unzip texinfo gcc build-essential
chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils
iputils-ping python3-git python3-jinja2 python3-subunit zstd liblz4-tool file
locales libacl1

0 项奖励
回复
3,680 次查看
timorkal
Contributor I

Thanks, but all those packages are already installed on my system:

ubuntu@yocto-build-server:~$ sudo apt install gawk wget git diffstat unzip texinfo gcc build-essential
utils-ping python3-git python3-jchrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils

Reading package lists... Doneon3-j
inja2 python3-subunit zstd liblz4-tool file
Building dependency tree... Done
Reading state information... Done
gawk is already the newest version (1:5.2.1-2build3).
wget is already the newest version (1.21.4-1ubuntu4.1).
git is already the newest version (1:2.43.0-1ubuntu7.2).
diffstat is already the newest version (1.66-1build1).
unzip is already the newest version (6.0-28ubuntu4.1).
texinfo is already the newest version (7.1-3build2).
gcc is already the newest version (4:13.2.0-7ubuntu1).
build-essential is already the newest version (12.10ubuntu1).
0 upgraded, 0 newly installed, 0 to remove and 0 not upgraded.

0 项奖励
回复
3,676 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Did you modify yocto recipes?

Please check whether "git-native" is listed in list "ASSUME_PROVIDED" in sources/poky/meta/conf/bitbake.conf.

What is the output when you run command "bitbake git-native"?

0 项奖励
回复
3,674 次查看
timorkal
Contributor I

yes git-native is part of the sources/poky/meta/conf/bitbake.conf file:

ASSUME_PROVIDED = "\
    bash-native \
    bzip2-native \
    chrpath-native \
    diffstat-native \
    file-native \
    findutils-native \
    gawk-native \
    git-native \
    grep-native \
    hostperl-runtime-native \
    hostpython-runtime-native \
    libgcc-native \
    patch-native \
    sed-native \
    tar-native \
    texinfo-native \
    virtual/crypt-native \
    virtual/libiconv-native \
    virtual/libintl-native \
    wget-native \
    "

 

This is the output of the bitback git-native command:

ubuntu@yocto-build-server:/mnt/disks/yocto_disk/imx-yocto-bsp$ bitbake git-native
WARNING: Host distribution "ubuntu-24.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended 
that you use a tested distribution.
Loading cache: 100% |#######################################################################################################################################| Time: 0:00:02Loaded 5730 entries from dependency cache.
Parsing recipes: 100% |#####################################################################################################################################| Time: 0:00:00Parsing of 3654 .bb files complete (3653 cached, 1 parsed). 5731 targets, 377 skipped, 3 masked, 0 errors.
WARNING: Explicit target "git-native" is in ASSUME_PROVIDED, ignoring
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION           = "2.8.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "universal"
TARGET_SYS           = "aarch64-poky-linux"
MACHINE              = "imx8mp-lpddr4-evk"
DISTRO               = "fsl-imx-xwayland"
DISTRO_VERSION       = "6.6-scarthgap"
TUNE_FEATURES        = "aarch64 armv8a crc crypto"
TARGET_FPU           = ""
meta
meta-poky            = "HEAD:200d12b6a58ad961d60a7774ca0f7a9d29498724"
meta-oe
meta-multimedia
meta-python          = "HEAD:72018ca1b1a471226917e8246e8bbf9a374ccf97"
meta-freescale       = "HEAD:0627128b341cfb2bef7a0832ce8cac0ce1127f13"
meta-freescale-3rdparty = "HEAD:6c063450d464eb2f380443c7d9af1b94ce9b9d75"
meta-freescale-distro = "HEAD:b9d6a5d9931922558046d230c1f5f4ef6ee72345"
meta-imx-bsp
meta-imx-sdk
meta-imx-ml
meta-imx-v2x         = "HEAD:219f6d04a4c339eb6f2dc626f944bbdf9a716ff5"
meta-nxp-demo-experience = "HEAD:e8e646e22b1f926aac83bb7ad522efa9cd8ccc45"
meta-nxp-matter-baseline
meta-nxp-openthread  = "HEAD:f58365ec75a5768ff3e8e8bcd64f237738c93160"
meta-arm
meta-arm-toolchain   = "HEAD:950a4afce46a359def2958bd9ae33fc08ff9bb0d"
meta-clang           = "HEAD:2b7433611d80f6d0ee1b04156fa91fc73d3c2665"
meta-gnome
meta-networking
meta-filesystems     = "HEAD:72018ca1b1a471226917e8246e8bbf9a374ccf97"
meta-qt6             = "HEAD:586a6cb5aec755803a3be3cec359baafe89d6432"
meta-parsec
meta-tpm             = "HEAD:459d837338ca230254baa2994f870bf6eb9d0139"
meta-virtualization  = "HEAD:6f3c1d8f90947408a6587be222fec575a1ca5195"


Summary: There were 2 WARNING messages.

 

0 项奖励
回复
3,630 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please go to folder "imx-yocto-bsp_scarthgap/build/tmp/work/x86_64-linux/git-native/2.44.1/git-2.44.1" and check whether you could run the following commands sucessfully.

$ make distclean

$ make -j 4 NO_PYTHON=1 CFLAGS='-isystem/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/include -O2 -pipe' LDFLAGS='-L/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib -L/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib -Wl,-rpath,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib -Wl,-rpath,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 -pthread' PERL_PATH='/usr/bin/env perl' COMPUTE_HEADER_DEPENDENCIES=no NO_GETTEXT=1 NO_CROSS_DIRECTORY_HARDLINKS=1

 

0 项奖励
回复
3,458 次查看
timorkal
Contributor I
I guess it helped, because I was managed to pass the git-native step afterwards.
0 项奖励
回复
3,615 次查看
timorkal
Contributor I

managed to build it successfully after adding these.
it gave me curl-config and git-gui issues without them.

sudo apt install libcurl4-openssl-dev libssl-dev gettext tcl-dev 



0 项奖励
回复
3,613 次查看
timorkal
Contributor I

Though, still retrying to build the bitback for imx8 fails on git-native.

ubuntu@yocto-build-server:/mnt/disks/yocto_disk/imx-yocto-bsp/build$ bitbake imx-image-full
WARNING: Host distribution "ubuntu-24.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended 
that you use a tested distribution.
Loading cache: 100% |#######################################################################################################################################| Time: 0:00:02Loaded 5730 entries from dependency cache.
Parsing recipes: 100% |#####################################################################################################################################| Time: 0:00:00Parsing of 3654 .bb files complete (3653 cached, 1 parsed). 5731 targets, 377 skipped, 3 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION           = "2.8.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "universal"
TARGET_SYS           = "aarch64-poky-linux"
MACHINE              = "imx8mp-lpddr4-evk"
DISTRO               = "fsl-imx-xwayland"
DISTRO_VERSION       = "6.6-scarthgap"
TUNE_FEATURES        = "aarch64 armv8a crc crypto"
TARGET_FPU           = ""
meta
meta-poky            = "HEAD:200d12b6a58ad961d60a7774ca0f7a9d29498724"
meta-oe
meta-multimedia
meta-python          = "HEAD:72018ca1b1a471226917e8246e8bbf9a374ccf97"
meta-freescale       = "HEAD:0627128b341cfb2bef7a0832ce8cac0ce1127f13"
meta-freescale-3rdparty = "HEAD:6c063450d464eb2f380443c7d9af1b94ce9b9d75"
meta-freescale-distro = "HEAD:b9d6a5d9931922558046d230c1f5f4ef6ee72345"
meta-imx-bsp
meta-imx-sdk
meta-imx-ml
meta-imx-v2x         = "HEAD:219f6d04a4c339eb6f2dc626f944bbdf9a716ff5"
meta-nxp-demo-experience = "HEAD:e8e646e22b1f926aac83bb7ad522efa9cd8ccc45"
meta-nxp-matter-baseline
meta-nxp-openthread  = "HEAD:f58365ec75a5768ff3e8e8bcd64f237738c93160"
meta-arm
meta-arm-toolchain   = "HEAD:950a4afce46a359def2958bd9ae33fc08ff9bb0d"
meta-clang           = "HEAD:2b7433611d80f6d0ee1b04156fa91fc73d3c2665"
meta-gnome
meta-networking
meta-filesystems     = "HEAD:72018ca1b1a471226917e8246e8bbf9a374ccf97"
meta-qt6             = "HEAD:586a6cb5aec755803a3be3cec359baafe89d6432"
meta-parsec
meta-tpm             = "HEAD:459d837338ca230254baa2994f870bf6eb9d0139"
meta-virtualization  = "HEAD:6f3c1d8f90947408a6587be222fec575a1ca5195"

Sstate summary: Wanted 5226 Local 0 Mirrors 0 Missed 5226 Current 2598 (0% match, 33% complete)###############################################              | ETA:  0:00:01Initialising tasks: 100% |##################################################################################################################################| Time: 0:00:15NOTE: Executing Tasks
ERROR: git-native-2.44.1-r0 do_compile: oe_runmake failed
ERROR: git-native-2.44.1-r0 do_compile: ExecutionError('/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/temp/run.do_compile.12690', 1, None, None)
ERROR: Logfile of failure stored in: /mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/temp/log.do_compile.12690
Log data follows:
| DEBUG: Executing python function autotools_aclocals
| DEBUG: SITE files ['endian-little', 'common-linux', 'common-glibc', 'bit-64', 'x86_64-linux', 'common']
| DEBUG: Python function autotools_aclocals finished
| DEBUG: Executing shell function do_compile
| NOTE: make -j 16 NO_PYTHON=1 CFLAGS=-isystem/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/include -O2 -pipe LDFLAGS=-L/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib                         -L/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib                         -Wl,--enable-new-dtags                         -Wl,-rpath-link,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib                         -Wl,-rpath-link,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib                         -Wl,-rpath,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/usr/lib                         -Wl,-rpath,/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/work/x86_64-linux/git-native/2.44.1/recipe-sysroot-native/lib                         -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/mnt/disks/yocto_disk/imx-yocto-bsp/build/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 -pthread PERL_PATH=/usr/bin/env perl COMPUTE_HEADER_DEPENDENCIES=no NO_GETTEXT=1 NO_CROSS_DIRECTORY_HARDLINKS=1        
|     * new build flags
|     CC oss-fuzz/dummy-cmd-main.o
| /bin/sh: 1: cc: not found
|     CC oss-fuzz/fuzz-commit-graph.o
| /bin/sh: 1: cc: not found
| make: *** [Makefile:2735: oss-fuzz/dummy-cmd-main.o] Error 127
| make: *** Waiting for unfinished jobs....
| make: *** [Makefile:2735: oss-fuzz/fuzz-commit-graph.o] Error 127
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (virtual:native:/mnt/disks/yocto_disk/imx-yocto-bsp/sources/poky/meta/recipes-devtools/git/git_2.44.1.bb:do_compile) failed with exit code '1'
0 项奖励
回复