Fail to read and write by NXP i.mx/Mscale DDR tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fail to read and write by NXP i.mx/Mscale DDR tool

Jump to solution
1,416 Views
justinfei
Contributor I

Hi,

    I have passed the DDR Stress test by NXP i.mx/Mscale DDR tool.But when I write 0x5A5A5A5A to the first address of DDR(0x00000000),I  read the address and the result is 0x14000100.It's different between the read value and the wrote value.

   1,Is there something wrong with use this tool?

   2,Does this mean that there is something wrong with the configuration of DDR parameters?

I use the two piece DDRs(one density is 8Gb,) in my system,so this system has 2GB DDR and 32bit data line.

Labels (1)
Tags (1)
0 Kudos
1 Solution
1,395 Views
BiyongSUN
NXP Employee
NXP Employee

Where is the first address of DDR(0x00000000) come from ? 

 

The memory mapping is in the reference manual. 

 

Untitled.png

View solution in original post

0 Kudos
4 Replies
1,396 Views
BiyongSUN
NXP Employee
NXP Employee

Where is the first address of DDR(0x00000000) come from ? 

 

The memory mapping is in the reference manual. 

 

Untitled.png

0 Kudos
1,412 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which product are you using?

0 Kudos
1,410 Views
justinfei
Contributor I

imx8mq

0 Kudos
1,397 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos