Fail to read and write by NXP i.mx/Mscale DDR tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Fail to read and write by NXP i.mx/Mscale DDR tool

跳至解决方案
4,411 次查看
justinfei
Contributor I

Hi,

    I have passed the DDR Stress test by NXP i.mx/Mscale DDR tool.But when I write 0x5A5A5A5A to the first address of DDR(0x00000000),I  read the address and the result is 0x14000100.It's different between the read value and the wrote value.

   1,Is there something wrong with use this tool?

   2,Does this mean that there is something wrong with the configuration of DDR parameters?

I use the two piece DDRs(one density is 8Gb,) in my system,so this system has 2GB DDR and 32bit data line.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
4,390 次查看
BiyongSUN
NXP Employee
NXP Employee

Where is the first address of DDR(0x00000000) come from ? 

 

The memory mapping is in the reference manual. 

 

Untitled.png

在原帖中查看解决方案

0 项奖励
回复
4 回复数
4,391 次查看
BiyongSUN
NXP Employee
NXP Employee

Where is the first address of DDR(0x00000000) come from ? 

 

The memory mapping is in the reference manual. 

 

Untitled.png

0 项奖励
回复
4,407 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which product are you using?

0 项奖励
回复
4,405 次查看
justinfei
Contributor I

imx8mq

0 项奖励
回复
4,392 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport
0 项奖励
回复