Fail to boot from NAND flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Fail to boot from NAND flash

跳至解决方案
11,085 次查看
wei-fonglin
Contributor II

Hi All,

Our product with i.MX6q system sometimes fail to boot from NAND flash.

I found a similar case(ERR007117) with this error in IMX6DQ errata document.

Is it a same situation with case ERR007117?

Debug log is as below.


U-Boot 2009.08-dirty ( 7月 02 2014 - 11:48:24)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz

Thermal sensor with ratio = 186

Temperature:   23 C, calibration data 0x5984fd69

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 264000000Hz

emi_slow clock: 29333333Hz

ddr clock     : 528000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 11000000Hz

Board: i.MX6Q-PCP-A301: unknown-board Board: 0x63012 [POR ]

Boot Device: NAND

I2C:   ready

DRAM:   1 GB

NAND:  gpmi_reset_block(00112000): module reset timeout

gpmi_reset_block(00112000): module reset timeout

gpmi_reset_block(00112000): module reset timeout

gpmi_reset_block(00112000): module reset timeout

gpmi_reset_block(00112000): module reset timeout

gpmi_reset_block(00112000): module reset timeout

gpmi_reset_block(00112000): module reset timeout

gpmi_reset_block(00112000): module reset timeout

gpmi_reset_block(00112000): module reset timeout

gpmi_reset_block(00112000): module reset timeout

[send_command] DMA error

Command execute failed!

[send_command] DMA error

Command execute failed!

[read_data] DMA error

[read_data] DMA error

[send_command] DMA error

Command execute failed!

[read_data] DMA error

[read_data] DMA error

[send_command] DMA error

Command execute failed!

[read_data] DMA error

[send_command] DMA error

Command execute failed!

[read_data] DMA error

[read_data] DMA error

[read_data] DMA error

[read_data] DMA error

[read_data] DMA error

[read_data] DMA error

[read_data] DMA error

[read_data] DMA error

No NAND device found!!!

0 MiB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2

标签 (1)
标记 (2)
1 解答
8,151 次查看
PeterChan
NXP Employee
NXP Employee

Yes, the error is caused by ENGR007117. You need i.MX6Q silicon rev 1.3 on your board and your u-boot need to follow the procedure in this errata to work around this issue. Example code can be found at setup_gpmi_nand() in Yocto L3.10.17 u-boot-imx/2013.04-r0/git/board/freescale/mx6qsabreauto/mx6qsabreauto.c (attached).

在原帖中查看解决方案

8 回复数
8,152 次查看
PeterChan
NXP Employee
NXP Employee

Yes, the error is caused by ENGR007117. You need i.MX6Q silicon rev 1.3 on your board and your u-boot need to follow the procedure in this errata to work around this issue. Example code can be found at setup_gpmi_nand() in Yocto L3.10.17 u-boot-imx/2013.04-r0/git/board/freescale/mx6qsabreauto/mx6qsabreauto.c (attached).

8,151 次查看
乐乐季
Contributor I

HI peterchan;

1."You need i.MX6Q silicon rev 1.3 on your board" is what meaning?

2.my page size is 4096,the OBB is 224,is it true?

3.mu uboot2013 can Operate Nand register,so it can recognize the nand ,but the uboot can't read/write the memory.

  It display :

MXS NAND: DMA read error

MXS NAND: Error sending command

0 项奖励
回复
8,151 次查看
PeterChan
NXP Employee
NXP Employee

1. Yes, you need i.MX6Q silicon rev 1.3 for NAND boot. All code that switch switching enfc_clk_root also needs to follow the procedure in errata.

2,3. The errata ENGR007117 does not related to NAND layout. The problem is the enfc_clk_root clock is not gated off before switching its clock source. The clock glitches might be passed to the dividers that follow and will affect the GPMI and BCH. Please double check your u-boot to ensure it is following the errata to switch enfc_clk_root.

0 项奖励
回复
8,151 次查看
乐乐季
Contributor I

HI peterchan:

1.I'm sorry to understand the "silicon",please explain again.

2.I reference you provide mx6qsabreauto.c, I operated the command in uboot:

     MX6QSABRELITE U-Boot > nand read 10800000 10000000 400000

     NAND read: device 0 offset 0x10000000, size 0x400000

but prompt:

MXS NAND: DMA read error

MXS NAND: Error sending command

3.  it doesn't matter with OOB size?

please! thank you!

0 项奖励
回复
8,151 次查看
PeterChan
NXP Employee
NXP Employee

The errata ENGR007117 describe a NAND boot problem caused by the enfc_clk_root clock is not gated off when doing clock source switching. The function blocks GPMI and IOMUX relies on the enfc_clk_root clock as its input. When power up, ROM code switches the enfc_clk_root clock source without gated off the clock to these blocks. clock glitches might be passed to the divider that follows the clock mux, and the divider might behave unpredictably. This can cause the clock generation to fail and the chip will not boot successfully.

The software workaround is to gate off the GPMI and IOMUX blocks before switching the enfc_clk_root clock source, and gate on these blocks again after switching complete. Silicon rev 1.3 has included this workaround to fix the problem in ROM code. So you need both silicon rev 1.3 and follow the ENGR007117 workaround in u-boot and kernel. Please refer to the chip errata document for more detail information.


Are you testing on silicon rev 1.3? Do you boot the i.MX6 chip from raw NAND? Or boot from other device and test the u-boot NAND commands? Can u-boot identify this NAND part?

0 项奖励
回复
8,153 次查看
madhutux
Contributor I

Hi PeterChan,

Thanks for pointing out the solution.,

BTW can you locate me the kernel fix for the same (for ERR007117)

and which branch contains the fix.

If possible, share the code as well.

0 项奖励
回复
8,153 次查看
乐乐季
Contributor I

HI peterchan:

my board is mx6q_sabrelit ; uboot is 2013.04;so I reference you provide the mx6qsabreauto.c, I added "setup_gpmi_nand(void)" at mx6qsabrelit.c,This function gated off ENFC_CLK_ROOT clock first ,then config gpmi and bch clock,and enable ENFC_CLK_ROOT clock,This function same as you above.

my uboot boot form SPI flash;This my uboot print info:

U-Boot 2013.04 (Jan 12 2015 - 18:51:10)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 32 C, calibration data: 0x55a4ae7d

Reset cause: POR

Board: MX6Q-Sabre Lite

I2C:   ready

DRAM:  1 GiB

NAND:  256 MiB     //my uboot can recognized Nand flash well.and parameters are correct!

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

SF: Detected SST25VF016B with page size 4 KiB, total 2 MiB

No panel detected: default to HDMI

unsupported panel HDMI

In:    serial

Out:   serial

Err:   serial

Net:   using phy at 7

FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  0

MX6QSABRELITE U-Boot > nand info

Device 0: nand0, sector size 128 KiB  //my nand parameters

  Page size      2048 b

  OOB size         64 b

  Erase size   131072 b

MX6QSABRELITE U-Boot > nand erase 0 400

NAND erase: device 0 offset 0x0, size 0x400

MXS NAND: DMA read error           //the DMA error

MXS NAND: Error sending command

MXS NAND: Error sending command

1."The silicon rev 1.3 " is the mx6q or uboot ? I'm sorry to understant it,can you give me the errata document? I don't know where download it.

2.I need to set the timing? I used the default timing at the uboot.and I used the Asynchronous.

0 项奖励
回复
8,153 次查看
PeterChan
NXP Employee
NXP Employee

You can download the i.MX6DQ errata at http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Documentation_Tab. You need i.MX6Q rev 1.3 when the boot device is NAND flash.

The MXS-NAND driver in u-boot 2013.04 does not update the GPMI_TIMINGx registers. These register values are either passed from the Firmware Configuration Block when boot mode is NAND or the reset values for other boot modes.

Since i.MX6Q is not boot from NAND and the u-boot can detect the NAND device, it does not seem your device is affected by ERR007117.

0 项奖励
回复