Hi NXP
My customer would like to implement Face recognition system on top of i.MX 8MM or 93.
Could you please recommend the appropriate reference example of face recognition?
I could find the opencv based Qt-C++ open sources from github.
I would appreciate if you able to provide an example project based on NXP which is able to easily integrated into i.MX Yocto Qt project.
Thanks.
Regards,
Adam
Solved! Go to Solution.
pls refer to the link as below:
FYI - a better example is available at nxp-nnstreamer-examples/face at main · nxp-imx/nxp-nnstreamer-examples.
Thanks Joanxie
pls refer to the link as below: