Face recognition on i.MX8MM/93

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Face recognition on i.MX8MM/93

Jump to solution
1,604 Views
Jack-Cha
Contributor V

Hi NXP 

My customer would like to implement Face recognition system on top of i.MX 8MM or 93.

Could you please recommend the appropriate reference example of face recognition?

I could find the opencv based Qt-C++ open sources from github.

I would appreciate if you able to provide an example project based on NXP which is able to easily integrated into i.MX Yocto Qt project.

Thanks.

Regards, 

Adam

0 Kudos
Reply
1 Solution
3 Replies
739 Views
pontikes
NXP Employee
NXP Employee
0 Kudos
Reply
1,579 Views
Jack-Cha
Contributor V

Thanks Joanxie

0 Kudos
Reply
1,593 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply