We try to set the fuses also in the demoboard of NXP (6SX-SABRE-SDB RevC), with the same result:
1- as you see picture above the configuration fuses is set to boot from SD by SD4, if I use MODE 0/1 to zero (boot from fuses mode )
the CPU doesn't boot
2- if I set the MODE 0/1 to 2 "boot from Intenal Boot" and set the
SW10 - 00000000
SW11 - 00111000
SW12 - 01000000
In this setting the CPU boot correctly from SD
We analyze signal in the first case and we don't see the SD4_CLK and SD4_CMD move ......
We read also SRC_SMBR1,2 and the values are correct.
It seems that the boot from fuses doesn't work.
Any suggestion ?