FSL Ubuntu 0912 Sources

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FSL Ubuntu 0912 Sources

965 次查看
Davros
Contributor III

Greetings Everyone,

When we received the iMX51 Babbage prototype board, there was an SD card with ubuntu on it, specifically the sticker on the back of the SD card mentions "FSL UBUNTU 0912".

I am trying to duplicate what is on the SD card, so I downloaded  the L2.6.31_09.12.01_SDK_source.  In its configuration there is an option for "FSL gnome release package", however nothing mentioned ubuntu.  

Please let me know what I need to download, or change in order to build this.

Many thanks,

Daryl W. Jarman

标记 (1)
0 项奖励
回复
1 回复

894 次查看
KursadOney
NXP Employee
NXP Employee

Hi Daryl,

My understanding is the Ubuntu SDK comes from Linaro. The linaro-linux-mx51 launchpad page might be a good place to start looking.

0 项奖励
回复