[FRDM imx93]: Not able to bring-up external mic to act as entry point for noise inputs.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[FRDM imx93]: Not able to bring-up external mic to act as entry point for noise inputs.

632件の閲覧回数
Aditya_Vashista
Contributor II

Hello,

I am trying to connect INMP441 MEMS High Precision Omnidirectional Microphone Module I2S with FRDM imx93 development board. In order to enable the mic via SAI3 for I2S interface by updating the device tree to modify functionality of GPIO pins. For this i have modified the device tree source file uploaded is test.dts (attached with this post). By testing it appears that the muxed clock doesn't seem to come on GPIO17(mclk). Also checked GPIO 16 AND 18 for TX_BCLK and RX_BCLK . Clock pulses are not coming.

On testing from software side using a gstreamer pipeline, i am still not able to get any input into the system.

 

I am attaching the conf file used to build the image as well as the modified device tree.

 

Thanks

Aditya Vashista

ラベル(3)
0 件の賞賛
返信
1 返信

612件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Do you have an additional device tree file?

Please confirm that you are using the correct pinmux values for used pads and verify that SAI3 peripheral clock is enabled.

cat /sys/kernel/debug/clk/clk_summary | grep sai

Best regards.

0 件の賞賛
返信