FIFO_RD_AUX_MSB read fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FIFO_RD_AUX_MSB read fails

1,636 Views
kimsangyoung
Contributor I

Deare anyone

I'm made new board useing i.mx6q cpu.

Lvds screen is normal behavior and normal boot .

After a check messages on the console the same message is printed below. What features do I have wrong output this message?

 

root@sabresd_6dq:/ # FIFO_RD_AUX_MSB read fails

 

FIFO_RD_AUX_LSB read fails

 

FIFO_RD_AUX_MSB read fails

 

FIFO_RD_AUX_LSB read fails

 

FIFO_RD_AUX_MSB read fails

 

FIFO_RD_AUX_LSB read fails

 

FIFO_RD_AUX_MSB read fails

 

Labels (1)
0 Kudos
Reply
3 Replies

863 Views
anegoiko
Contributor III

Hi Kim

I'm getting the same message and I don't know which kernel boot parameter I should check. Did you solve the problem?

0 Kudos
Reply

863 Views
wangwenxue1989
Contributor I

set CONFIG_TOUCHSCREEN_MAX11801 in .config file as no

0 Kudos
Reply

863 Views
igorpadykov
NXP Employee
NXP Employee

Hi kim

these messages are from drivers/input/touchscreen/max11801_ts.c

driver, probably you should recheck kernel boot parameters

Best regards

igor

0 Kudos
Reply