Hello,
We are trying to unlink the pca9534pwr from the FEC ethernet interface as we will not incorporate it in our project. We just changed the rst and vsel pins in our normal boot and uboot device tree. It seems to work when the PCA9534 is still on the board and connected to the ethernet 1 interface. But as soon as we remove it from the evaluation board, and then attach new pins to the vsel and rst lines it stops working.It seems that the transceiver output is not working, but following the line of vsel, it seems to be perfectly connected. I include it here in case someone can see a malfunction of the system. I also attach the dts files that we have changed.
Thank you,
César.