FEC_MIIGSK_CFGR and FEC_MIIGSK_ENR registers not documented in RM or datasheet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FEC_MIIGSK_CFGR and FEC_MIIGSK_ENR registers not documented in RM or datasheet

961 次查看
bikenomad
Contributor IV

In the i.mx53RM and i.mx53IEC manuals, I can't find any documentation of the bits within the FEC_MIIGSK_CFGR and FEC_MIIGSK_ENR registers.

The following bits are referred to in the manual but not documented. I have added what I think from reading the Linux sources is the correct positions, but am not sure.

FEC_MIIGSK_CFGR (0x63FE_C300):

  • I/F_MODE bit[1:0], 01=RMII, 00=MII
  • FRCONT  bit6, 1=force 10Mbps
  • LBMODE

FEC_MIIGSK_ENR (0x63FE_C308)

  • EN bit1
  • READY  bit2, r/o

What is the correct definition of these registers?

Also, can someone make a note to fix the manuals?

Thanks...

0 项奖励
回复
3 回复数

631 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 Your definition of the registers is correct.

1.png

2.png

3.png

Regards,

Yuri.

0 项奖励
回复

631 次查看
EdSutter
Senior Contributor II
0 项奖励
回复

631 次查看
EdSutter
Senior Contributor II

Did you ever figure this out?  I have the same question, and will be posting to other groups shortly.

0 项奖励
回复