External memory configurations for iMX8MPlus to its core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External memory configurations for iMX8MPlus to its core

1,357件の閲覧回数
ReshmaRoy
Contributor II

There are External memories such as LPDDR, eMMC and Flash. Among these which all memories are for A53 core and M7 core of iMX8MPlus SoC.

0 件の賞賛
返信
4 返答(返信)

1,343件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @ReshmaRoy!

Thank you for contacting NXP Support!

The LPDDR can be used by both cores.

The eMMC/Flash memory is needed to boot the processor, Once booted the M7 binary can be loaded from eMMC/Flash memory and run in TCM or DRAM.

 

To understand better the boot process of the iMX8MP you can consult the reference manual on chapter 6.1 (System Boot).

 

Best Regards!

Chavira

0 件の賞賛
返信

1,327件の閲覧回数
ReshmaRoy
Contributor II

So, It means that we require either eMMC or Flash right? We don't require both memories in the design right?

0 件の賞賛
返信

1,320件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @ReshmaRoy!

Yes, you are right!

 

To boot the processor you need only one.

 

 

0 件の賞賛
返信

1,240件の閲覧回数
ReshmaRoy
Contributor II

Thankyou for the support.