External memory configurations for iMX8MPlus to its core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External memory configurations for iMX8MPlus to its core

952 Views
ReshmaRoy
Contributor II

There are External memories such as LPDDR, eMMC and Flash. Among these which all memories are for A53 core and M7 core of iMX8MPlus SoC.

0 Kudos
Reply
4 Replies

939 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @ReshmaRoy!

Thank you for contacting NXP Support!

The LPDDR can be used by both cores.

The eMMC/Flash memory is needed to boot the processor, Once booted the M7 binary can be loaded from eMMC/Flash memory and run in TCM or DRAM.

 

To understand better the boot process of the iMX8MP you can consult the reference manual on chapter 6.1 (System Boot).

 

Best Regards!

Chavira

0 Kudos
Reply

923 Views
ReshmaRoy
Contributor II

So, It means that we require either eMMC or Flash right? We don't require both memories in the design right?

0 Kudos
Reply

916 Views
Chavira
NXP TechSupport
NXP TechSupport

HI @ReshmaRoy!

Yes, you are right!

 

To boot the processor you need only one.

 

 

0 Kudos
Reply

836 Views
ReshmaRoy
Contributor II

Thankyou for the support.