External contacts ONOFF and POR_B microcontroller MIMXRT1176

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External contacts ONOFF and POR_B microcontroller MIMXRT1176

Jump to solution
703 Views
muxeu
Contributor II

Hello.
Please tell me what can be done with the external contacts ONOFF (U10) and POR_B (T10) of the MIMXRT1176 microcontroller, if I am not going to use them for their intended purpose? Unfortunately, section 3.2 of IMXRT1170AEC.pdf does not say anything about them.

0 Kudos
1 Solution
690 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @muxeu ,

If not used, ON/OFF can be a no-connect.

The POR_B can be a no-connect too. POR_B has a 100k internal pull-up resistor to SNVS domain.  In the absence of an external reset feeding the POR_B input, the internal POR module takes control. But it's recommended to add the external reset IC to the circuit to guarantee POR_B is properly processed during power up/down.

 

Regards,

Jing

View solution in original post

0 Kudos
2 Replies
691 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @muxeu ,

If not used, ON/OFF can be a no-connect.

The POR_B can be a no-connect too. POR_B has a 100k internal pull-up resistor to SNVS domain.  In the absence of an external reset feeding the POR_B input, the internal POR module takes control. But it's recommended to add the external reset IC to the circuit to guarantee POR_B is properly processed during power up/down.

 

Regards,

Jing

0 Kudos
683 Views
muxeu
Contributor II

Thank you for the answers.

0 Kudos