I have a custom IMXDL board with a KSZ8863 switch.
According to MDIO the switch is fine, but RMII is dead silent.
Both IMXDL and PHY are clocked by external clock.
I would like to confirm that it is indeed possible to use RGMII_TX_CTL to clock RMII from an external clock?
The HW dev. guide (IMX6DQ6SDLHDG) is a bit light on detail regarding RGMII_TX_CTL, as GPIO_16 is the recommended external clock sink.
If RGMII_TX_CTL is a valid clock sink for RMII, it's a SW issue and I'd much appreciate any sample code.
I'm trying to get ethernet running on uboot, for a start.
已解决! 转到解答。
Hi Magnus
yes this signal also can be used for RMII as described in
IMX6SDLRM Table 23-1. ENET External Signals
There are some RMII examples below
Re: RMII interface on i.MX6 Solo
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Magnus
yes this signal also can be used for RMII as described in
IMX6SDLRM Table 23-1. ENET External Signals
There are some RMII examples below
Re: RMII interface on i.MX6 Solo
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------