Hello there,
Happy New Year! I can't setup manual exposure with gstreamer on my OV5640 camera running with a SabreLite imx6 board.
Bellow is my test pipeline, no matter what value of exposure time I enter, the exposure is the same:
#gst-launch-1.0 imxv4l2videosrc device=/dev/video1 exposure-time=30 ! imxeglvivsink
Thanks!
-Luca
Hi Luca
gstreamer-imx is developed and supported by community and one can post
it on meta-fsl-arm mailing list, so that someone familiar with that version could try to assist
https://lists.yoctoproject.org/listinfo/meta-freescale
more details can be found on
trac.gateworks.com/wiki/Yocto/gstreamer
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you, Igor.
I subscribed to the community that you recommended and am awaiting approval. By the way, the community you recommend supports Yocto but I'm using Ubuntu, I hope they can help me with this gstreamer exposure setting problem in the SabreLite board because I'm running out of options :smileysad:.
-Luca