Expected Data Format for VpuBufferNode VPU Wrapper

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Expected Data Format for VpuBufferNode VPU Wrapper

980件の閲覧回数
hsuq7052
Contributor II

I'm using an IMX.8MP trying to use the VPU Wrapper. I have a RTP stream of H.264 Encoded Video of Fragmented FU-A NALU's along with SPS and PPS NALUs. The stream is non-interleaved with the fragmented NALU's having a nal_unit type of 5 (coded slice of an IDR picture). How should I process the stream data into the VpuBufferNode to then decode. I've tried removing the first 12 bytes which represent the RTP header info and passing the rest into the decoder. Ive been reading RTP Payload Format for H.264 Video which says I should preform a de-packetization process in which I concatenate the fragmented FU payloads of a fragmented NALU together and then send that to the decoder. Is that what I should be assigning to the VpuBufferNode? Also how would I process SPS and PPS NALUs and to send to the decoder?

ラベル(1)
0 件の賞賛
返信
1 返信

959件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Sorry no SPS and PPS form MX8 VPU, may be useful to look at updated for i.MX8

i.MX_VPU_Application_Programming_Interface_Linux_Reference_Manual

 

Regards

0 件の賞賛
返信