Exceptional / unexpected termination of video stream on imx51/Linux-2.6.31

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Exceptional / unexpected termination of video stream on imx51/Linux-2.6.31

1,261 Views
RobbieJiang
Contributor IV

Hi all,

I have a gstreamer pipeline working on i.mx51/Linux-2.6.31:

mfw_v4lsrc sensor-width=720 sensor-height=288 capture-width=640 capture-height=480 preview=true preview-width=640 preview-height=480 ! 'video/x-raw-yuv, format=(fourcc)NV12, width=640, height=480, framerate=25/1' ! clockoverlay ! mfw_vpuencoder codec-type=std_avc width=640 height=480 ! filesink location=video.264

However, after some time ( e.g, several hours), the pipeline terminates with one of  the following three kinds of message:

1.

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x01000000

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x02000000

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_5 = 0x00100000

mxc_ipu mxc_ipu: handler already installed on irq 451

mxc_ipu mxc_ipu: DC irq 451 in use

mxc_v4l_close: release resource

ERROR: v4l2 capture: camera_callback: working queue empty

OR

2.

ERROR: v4l2 capture: mxc_v4l_dqueue() interrupt received

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x02000000

mxc_v4l_close: release resource

OR

3.

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

mxc_v4l_close: release resource

By the way, the video source is from a tvin chip ( TVP 5150).

And the  VPU firmware is 15.3.10, libvpu version is 5.0.).

What's the meaning of these error messages?

Is there anything wrong with my tvin driver?

Or should I upgrade the vpu firmware and libvpu?

Cheers,

Robbie

Labels (3)
0 Kudos
Reply
1 Reply

825 Views
Yuri
NXP Employee
NXP Employee

Hello,

Please refer to the following

https://community.nxp.com/thread/274730#comment-322666

Regards,

Yuri.

0 Kudos
Reply