Example for using CCM_CLKO1 on i.MX7D?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example for using CCM_CLKO1 on i.MX7D?

ソリューションへジャンプ
2,143件の閲覧回数
skrap
Contributor IV

Hello,

I'm a bit confused as to how the i.MX7d's CCM_CLKO1 and CCM_CLKO2 are intended to be used.  I see that there are entries in the devtree bindings for the root src, the dividers, etc, but I don't see the expected entries for the clocks themselves.

#define IMX7D_CLKO1_ROOT_SRC       338
#define IMX7D_CLKO1_ROOT_CG       339
#define IMX7D_CLKO1_ROOT_DIV      340
#define IMX7D_CLKO2_ROOT_SRC      341
#define IMX7D_CLKO2_ROOT_CG       342
#define IMX7D_CLKO2_ROOT_DIV      343
#define IMX7D_CLKO1_ROOT_PRE_DIV    406
#define IMX7D_CLKO2_ROOT_PRE_DIV   407

I would also expect to see IMX7D_CLKO1_ROOT_CLK and IMX7D_CLKO2_ROOT_CLK.  Is it hiding somewhere that I haven't found yet?  Or is there a different name for those clocks?

More broadly, is there an example of these clocks being used anywhere?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,894件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jonah

one can check similar issue

i.MX7D 24MHz clock output to CCM_CLK1_P pin 

and linux/Documentation/devicetree/bindings/clock/clock-bindings.txt

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,895件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jonah

one can check similar issue

i.MX7D 24MHz clock output to CCM_CLK1_P pin 

and linux/Documentation/devicetree/bindings/clock/clock-bindings.txt

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信