Ethernet on QWKS-SCMIMX6DQ with QWKS-ETHACC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet on QWKS-SCMIMX6DQ with QWKS-ETHACC?

979 Views
ronb127
Contributor I

Hello,

I'm using a QWKS-SCMIMX6DQ "Quick Start Board" with a QWKS-ETHACC daughter-board for ethernet access.

I've followed the exact instruction at:

https://www.nxp.com/docs/en/user-guide/QWKSEACSG.pdf 

But when I connect the ethernet cable the led on the connector remains OFF and "ifconfig" doesn't list any "eth0" interface (only loopback).

The 3V3_LED on the ETHACC is ON but it seems like the card is not operating.

Is it possible that I'm missing some kernel driver? I'm using the default microSD card supplied with the "Quick Start Board".

QWKS-ETHACC only works with Rev >= C, mine is Rev D.

Thanks,

Ron

Labels (1)
0 Kudos
4 Replies

628 Views
bobsmith1
Contributor I

I have the same problem using the ethacc with the qwks board.

Although the system sees and configures the ethernet interface

using the sdcard image mentioned, a reset of the board causes

the system to go into an endless loop of

   IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
   fec 2188000.ethernet eth0: Link is Down
   IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

The kernel is 4.1.15-2.0.0+g7a75e7f

The boards are

QWKS-ETHACC Rev X3 (per the box)

QWKS-ETHACC, SCH-29206 REV A

QWKS-ETHACC, 700-29206 REV X1

QWKS-SCMIMX6DQ, SCH-28927 REV D

QWKS-SCMIMX6DQ, 700-28927 REV B

What is going on?

0 Kudos

628 Views
bobsmith1
Contributor I

Got it.  The problem was a flaky ETHACC board.

The problem disappears completely with a second ETHACC.

0 Kudos

628 Views
ronb127
Contributor I

Works like a charm, thanks!

(I just used wayland/fsl-image-qt5-imx6dqscm-1gb-qwks-rev3.sdcard from the demo images.)

0 Kudos

628 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ron

please try with Demo Images

Board Support Packages (3)
Demo Images - QWKS Board based on SCM-i.MX 6D/Q(REV C)
L4.1.15_2.0.0-SCM-MX6DQ-C

Quick Start Board for SCM-i.MX 6DQ|NXP 

https://community.nxp.com/docs/DOC-333955 

For programming images one can use Mfg Tool on the same link.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos