Hello,
I just start working on Linux and imx6ul evaluation kit.
I connect my host machine (Ubuntu 14.04 LTS) with the board via USB to UART using connector J1901.
It is working fine and I can use board Shell via minicom. However When I connect the board in network switch via using Ethernet straight cable, I can see following activity on my board...
imx6ulevk:~$ fec 20b4000.ethernet eth0: Link is Up - 10Mbps/Half - flow controlf
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
fec 20b4000.ethernet eth0: Link is Down
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
fec 20b4000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
fec 20b4000.ethernet eth0: Link is Down
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
fec 20b4000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
fec 20b4000.ethernet eth0: Link is Down
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
Now my problem is...
1. Which are setting required to connect board Ethernet with host machine?
2. Which Ethernet cable I required to connect with host? Straight or cross ?
3. How do I send project file to the board via UART (USB to UART) ?
I have not change anything on board kernel, It is as per I received with the board in micro SD card.
Note: I do not have LCD display, I am using board terminal on my host machine.
Please help.
Regards
Jaydeep
HI Parmar,
We have been facing same problem with etho and eth1 and able to communicate with USB and UART. Problem is with ethernet data access, unable to ping but able to up. While the same cable physical connections were correct and able to ping for other PC but not to my iMX6Ultralite.
if any Suggestions please let us know.
Thanking You,
NagaPrasad
Please check the connection thoroughly. Please try to use another cable, hub, etc.
I just checked both eth0 and eth1 interfaces on our board and they are working fine. I was able to ping the outside.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
There is not any hardware issue as our machine is connected with internet or other embedded board (Phyboard-wega) too. We are having two i.MX6UL-EVK, and we tried this on both but the result was not favourable in any board.
Please review our following configuration which is same in both the boards,
root@imx6ulevk:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:04:9F:04:B4:D2
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
eth1 Link encap:Ethernet HWaddr 00:04:9F:04:B4:D3
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:10 errors:0 dropped:0 overruns:0 frame:0
TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:700 (700.0 B) TX bytes:700 (700.0 B)
root@imx6ulevk:~#
We have tried to configure the board through variety of ways including mentioned by you (igconfig eth0 ...).
I have copied /etc/network/interfaces file below for your reference,
# /etc/network/interfaces -- configuration file for ifup(8), ifdown(8)
# The loopback interface
auto lo
iface lo inet loopback
# Wireless interfaces
iface wlan0 inet dhcp
wireless_mode managed
wireless_essid any
wpa-driver wext
wpa-conf /etc/wpa_supplicant.conf
iface atml0 inet dhcp
# Wired or wireless interfaces
auto eth0
iface eth0 inet dhcp
iface eth1 inet dhcp
# Ethernet/RNDIS gadget (g_ether)
# ... or on host side, usbnet and random hwaddr
iface usb0 inet static
address 192.168.7.2
netmask 255.255.255.0
network 192.168.7.0
gateway 192.168.7.1
# Bluetooth networking
iface bnep0 inet dhcp
Looking forward for respond.
Regards
Jaydeep Parmar
Hi Victor,
I have already tested physical links, It is working fine on other machines.
I have not make any change in prebuilt image i got with the board in sdcard, if any change in it please share.
I tried to patch as mentioned in thread Patch to support Ethernet PHY KSZ8081 (Rev1) on i.MX6UL/i.MX6ULL EVK board
Please let me know if any other change in this or alternative way to debug it.
Regards
Jaydeep
Hi Victor,
I have already tested physical links, It is working fine on other machines.
I have not make any change in prebuilt image i got with the board in sdcard, if any change in it please share.
I tried to patch as mentioned in thread https://community.nxp.com/docs/DOC-333163
Please let me know if any other change in this or alternative way to debug it.
Regards
Jaydeep