Ethernet does not work on my MX50 EVK board Rev D -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet does not work on my MX50 EVK board Rev D -blog archive

397 Views
PeterChan
NXP Employee
NXP Employee

This is because the DCDC 3V15 on the EVK board has not enable yet. The ethernet port, which is powered by the DCDC, will not function until the DCDC has turned on.

It is unfortunately that the control logic of DCDC 3V15 in BSP release L2.6.35_11.04.01_ER is reverse to that required by the EVK board. The BSP should set the GPIO4_16 pin to level '1' instead of '0' to enable DCDC 3V15. The patch

L2.6.35_11.04.01_ER__mx50_rd3_DCDC3V15_fix.zip here should address this problem.

Tags (1)
0 Kudos
0 Replies