Ethernet data link does not work with MIMXRT1062

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet data link does not work with MIMXRT1062

2,794 次查看
Sha_G
Contributor I

Hello,

We are using the MIMXRT1062 on a custom board to communicate with the network.

Accordingly configured the ethernet port and registers in the firmware to do so. I had the link up and running until few days ago. And in between was working on some RTOS and mBedTls stuff. 

Now if I check, the ethernet port does not work ( data read back from PHY Read fails and shows that the link is down ).
Similarly the " PHY_GetAutoNegotiationStatus " and " PHY_GetLinkStatus " as used in the EVK example do not set the link up.
This is happening even when I am using my base code ( similar to the EVK example ) that I had used to verify ethernet earlier.
Wondering if any of the PHY settings/configurations have been changed ? This is a pretty urgent requirement.
Any help will be much appreciated.

标签 (1)
0 项奖励
回复
3 回复数

2,754 次查看
pauricacre
Contributor III

It may be a caching issue depending on your project configuration (ie using external SDRAM). Try disabling/commenting 

SCB_EnableDCache(); and SCB_EnableICache(); in BOARD_ConfigMPU(). This may point you in the right direction. This was another issue I had that was working previously in the demo projects.

 

0 项奖励
回复

2,762 次查看
Sha_G
Contributor I

PHY_AUTONEGO_TIMEOUT_COUNT is set to 100000 in my code.

Stepping through the debugger shows me that the data read from the SMI register ( MMFR ) seems to be different than what is expected - Causing the Auto Nego and Link status to not pass. The ST, OP, Pa, RA amd TA fields are all correct in the MMFR register. Just the DATA looks different than what could make the MDIO_Read to return a correct regValue. 

0 项奖励
回复

2,769 次查看
pauricacre
Contributor III

Have you changed the PHY_AUTONEGO_TIMEOUT_COUNT? Mine seems to stop working when I reduce this value from 100000 to 1000. When no ethernet cable is connected on mine it was stalling my application and this value was the holdup. So I need to come up with another solution. But as soon as I increase this value Ethernet works fine again.

0 项奖励
回复