Ethernet configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet configuration

2,090 Views
adityaprajapati
Contributor I

I want to communicate to the i.mx6UL board using ssh connection from my pc but when i try to connect the Ethernet the terminal shows following msgs 

IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
fec 20b4000.ethernet eth0: Link is Down
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
fec 20b4000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
fec 20b4000.ethernet eth0: Link is Down
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
fec 20b4000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
fec 20b4000.ethernet eth0: Link is Down
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
fec 20b4000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
fec 20b4000.ethernet eth0: Link is Down
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
fec 20b4000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

can anyone please guide me to configure the ethernet connection of this board 

Thank you 

With Regards 

Aditya

Labels (1)
0 Kudos
Reply
1 Reply

1,467 Views
b36401
NXP Employee
NXP Employee

Please check the connection thoroughly.
Please try to use another cable, hub, etc.

We checked both eth0 and eth1 interfaces on our i.MX6UL EVK board running Linux demo image and they are working fine.
We were able to ping the outside.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply