Ethernet PHY not working in yocto linux - i.MX8MM & DP83867IR/CR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet PHY not working in yocto linux - i.MX8MM & DP83867IR/CR

961 Views
tofu
Contributor I

We had a working project in qbase2 karo board that used the SoM QS8M-MQ00 (i.MX8MM) & KSZ9131RNX RGMII and it has been working without a problem. We're working with yocto linux.

When trying to adapt the yocto project to our custom board we're having problems with the use of DP83867IR/CR (eth0), we've managed to ping to the network with another chip on the board an USB-Eth one using eth1.

In order to configure for use we've added the following configurations to the kernel.

 

CONFIG_MII=y
CONFIG_DP83867_PHY=y

 

We've also modified the device tree files for both the u-boot and linux. This is our .dts for the kernel, we have the same in u-boot.

 

#include "imx8mm-qs8m-mq00.dts"
#include <dt-bindings/net/ti-dp83867.h>

/ {
	model = "TEST";
};

&fec1 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&pinctrl_fec1_b &pinctrl_etnphy_rst_b>;
	pinctrl-1 = <&pinctrl_fec1_b_sleep>;
	phy-mode = "rgmii";
	phy-handle = <&ethphy1>;
	phy-supply = <&reg_vdd_3v3>;
	// phy-reset-gpios = <&gpio2 12 GPIO_ACTIVE_LOW>;
	// phy-reset-duration-us = <25000>;
	// phy-reset-post-delay-us = <250000>;
	status = "okay";

	mdio0 {
    	#address-cells = <1>;
      	#size-cells = <0>;
      	ethphy1: ethernet-phy@0 {
			compatible = "ethernet-phy-ieee802.3-c22";
        	reg = <0>;
        	tx-fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
        	//rx-fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
        	ti,clk-output-sel = <DP83867_CLK_O_SEL_OFF>;
        	ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_25_NS>;
        	ti,tx-internal-delay = <DP83867_RGMIIDCTL_2_75_NS>;
      	};
	};
};

&iomuxc {
	// pinctrl_etnphy_int_b: etnphy-int-bgrp {
	// 	fsl,pins = <
	// 		    MX8MM_IOMUXC_GPIO1_IO10_GPIO1_IO10		0x90
	// 	>;
	// };

	pinctrl_etnphy_rst_b: etnphy-rst-bgrp {
		fsl,pins = <
			    MX8MM_IOMUXC_SD2_CD_B_GPIO2_IO12		0x140
		>;
	};

	pinctrl_fec1_b: fec1-bgrp {
		fsl,pins = <
			    MX8MM_IOMUXC_ENET_MDC_ENET1_MDC		0x142
			    MX8MM_IOMUXC_ENET_MDIO_ENET1_MDIO		0x142
			    MX8MM_IOMUXC_ENET_TXC_ENET1_RGMII_TXC	0x010
			    MX8MM_IOMUXC_ENET_TD0_ENET1_RGMII_TD0	0x016
			    MX8MM_IOMUXC_ENET_TD1_ENET1_RGMII_TD1	0x016
			    MX8MM_IOMUXC_ENET_TD2_ENET1_RGMII_TD2	0x016
			    MX8MM_IOMUXC_ENET_TD3_ENET1_RGMII_TD3	0x016
			    MX8MM_IOMUXC_ENET_RD0_ENET1_RGMII_RD0	0x150 /* MODE0 */
			    MX8MM_IOMUXC_ENET_RD1_ENET1_RGMII_RD1	0x150 /* MODE1 */
			    MX8MM_IOMUXC_ENET_RD2_ENET1_RGMII_RD2	0x150 /* MODE2 */
			    MX8MM_IOMUXC_ENET_RD3_ENET1_RGMII_RD3	0x150 /* MODE3 */
			    MX8MM_IOMUXC_ENET_RXC_ENET1_RGMII_RXC	0x116 /*qbase 4 0x156 */
			    MX8MM_IOMUXC_ENET_RX_CTL_ENET1_RGMII_RX_CTL	0x116 /*qbase 4 0x156 */
			    MX8MM_IOMUXC_ENET_TX_CTL_ENET1_RGMII_TX_CTL	0x016 
		>;
	};

	pinctrl_fec1_b_sleep: fec1-b-sleep-grp {
		fsl,pins = <
			    MX8MM_IOMUXC_ENET_MDC_GPIO1_IO16		0x120
			    MX8MM_IOMUXC_ENET_MDIO_GPIO1_IO17		0x120
			    MX8MM_IOMUXC_ENET_TXC_GPIO1_IO23		0x120
			    MX8MM_IOMUXC_ENET_TD0_GPIO1_IO21		0x120
			    MX8MM_IOMUXC_ENET_TD1_GPIO1_IO20		0x120
			    MX8MM_IOMUXC_ENET_TD2_GPIO1_IO19		0x120
			    MX8MM_IOMUXC_ENET_TD3_GPIO1_IO18		0x120
			    MX8MM_IOMUXC_ENET_RD0_GPIO1_IO26		0x120
			    MX8MM_IOMUXC_ENET_RD1_GPIO1_IO27		0x120
			    MX8MM_IOMUXC_ENET_RD2_GPIO1_IO28		0x120
			    MX8MM_IOMUXC_ENET_RD3_GPIO1_IO29		0x120
			    MX8MM_IOMUXC_ENET_RXC_GPIO1_IO25		0x120
			    MX8MM_IOMUXC_ENET_RX_CTL_GPIO1_IO24		0x120
			    MX8MM_IOMUXC_ENET_TX_CTL_GPIO1_IO22		0x120
		>;
	};
};

 

We know that the RGMII chip is working because from u-boot we can actually access the mdio and read all the registers. But linux doesn't seem to be able to find the PHY. I've tried to add a static IP to u-boot and ping from there, but that's also not working. Also, when adding the rest into the .dts u-boot stops detecting the PHY, but the reset pin seems to be ok. Any ideas?

 

0 - Generic PHY <--> ethernet@30be0000
QS8M U-Boot > mdio list
FEC0:
0 - Generic PHY <--> ethernet@30be0000
QS8M U-Boot > mii device
MII devices: 'FEC0' 
Current device: 'FEC0'

 

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

916 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @tofu,

I hope you are doing well
 
Kindly try to add the below compatible string to the device tree to bind the particular device.
compatible = "ethernet-phy-id2000.a231", "ethernet-phy-ieee802.3-c22";
 
Thanks & Regards,
Dhruvit Vasavada
0 Kudos
Reply