Ethernet AR8031 rate changes from 100M to 10M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet AR8031 rate changes from 100M to 10M

1,053件の閲覧回数
nickruan
Contributor II

Hi Supporter,

iMx6q board is connected to 100M switcher,

Ethernet chip si AR8031, the AR8031 can know the 100M network, but it's easy change to 10M rate.

It seems 100M is not stable, why

0 件の賞賛
返信
1 返信

823件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi nick

this may be caused by transmission errors, so one can try to use

more short and quality cables.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信