Eth for IMX6SLX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Eth for IMX6SLX

458 Views
luongtran
NXP Employee
NXP Employee

Dear all,

I developed Eth driver on IMX6Quad and it was working but It was not working on IMX6SLX board after I ported it to IMX6SLX. I could control PHY via LEDs under ETH port but it seems the messages were not transmitted out because I saw buffer flag but did not see transmit flag.

do you have any ideas to fix this problems? do you have any Eth sample code for IMX6SLX board?

Regards,

Luong

Labels (1)
0 Kudos
1 Reply

362 Views
igorpadykov
NXP Employee
NXP Employee

Hi Luong

one can look at uboot sources

uboot-imx.git - Freescale i.MX u-boot Tree 

and check attached Linux Manual Chapter 43 FEC Driver

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos