Errors while download image to the i.mxSolo target board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Errors while download image to the i.mxSolo target board

Jump to solution
1,281 Views
liquanduan
Contributor III

I use "bitbake fsl-image-mfgtool-initramfs"  command to get a u-boot-mfgtool***.imx version from "image/boot/", but ddr caliration parameters was not fit for current target. So burn failed!

Then I copy uboot(2016.03-r0) source code, modify the caliration paramters(from ddr_stress_tester tool ) in "uboot_source/board/freescale/mx6sabresd/mx6solo_4x_mt41j128.cfg" ;

Then execute

"make mx6dlsabresd_defconfig "

but this uboot.imx seems not fit for the mfgtool firmware.

 

/////log message as follow:

U-Boot 2016.03 (Jul 04 2017 - 21:24:08 -0400)

 

CPU:   Freescale i.MX6DL rev1.1 at 792MHz
CPU:   Commercial temperature grade (0C to 95C) at 50C
Reset cause: POR
Board: MX6-SabreSD
I2C:   ready
DRAM:  512 MiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

 

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc2(part 0) is current device
Net:   Board Net Initialization Failed
No ethernet found.
Boot from USB for mfgtools
Use default environment for                              mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot:  0
Kernel image @ 0x12000000 [ 0x000000 - 0x5579d0 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
   Image Name:   fsl-image-mfgtool-initramfs-imx6
   Image Type:   ARM Linux RAMDisk Image (gzip compressed)
   Data Size:    7565864 Bytes = 7.2 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
   Booting using the fdt blob at 0x18000000
   Using Device Tree in place at 18000000, end 1800e485
No PMIC found!

 

Starting kernel ...

 

Booting Linux on physical CPU 0x0
Linux version 4.1.15 (detc@detc) (gcc version 5.3.0 (GCC) ) #2 SMP PREEMPT Tue Jul 4 06:21:04 EDT 2017
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 DualLite SABRE Smart Device Board
Reserved memory: created CMA memory pool at 0x1c000000, size 320 MiB
Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @8bb1d000 s16716 r8192 d24244 u49152
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendf
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 173316K/524288K available (6911K kernel code, 324K rwdata, 2364K rodata, 400K init, 424K bss, 23292K reserved, 327680K cma-reserved, 0K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0xa0800000 - 0xff000000   (1512 MB)
    lowmem  : 0x80000000 - 0xa0000000   ( 512 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .text : 0x80008000 - 0x80917058   (9277 kB)
      .init : 0x80918000 - 0x8097c000   ( 400 kB)
      .data : 0x8097c000 - 0x809cd140   ( 325 kB)
       .bss : 0x809d0000 - 0x80a3a194   ( 425 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Preemptible hierarchical RCU implementation.
        Additional per-CPU info printed with stalls.
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS:16 nr_irqs:16 16
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 512 kB
L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76450001
mxc_clocksource_init 3000000
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10008280 - 0x100082f0
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated (12.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
CPU identified as i.MX6DL, silicon rev 1.1
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6dl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
mxs-dma 110000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7392K (82c00000 - 83338000)
CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 512 (order: 3, 32768 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
mxc_sdc_fb fb@0: NO mxc display driver found!
mxc_sdc_fb fb@1: NO mxc display driver found!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 1-0008: unrecognized pfuze chip ID!
imx-sdma 20ec000.sdma: loaded firmware 3.3
pfuze100-regulator: probe of 1-0008 failed with error -5
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 25, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
m25p80 spi0.0: unrecognized JEDEC id bytes: 00,  0,  0
spi_imx 2008000.ecspi: probed
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 26:a5:83:81:3c:78
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184000.usb supply vbus not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
LUN: removable read only file: /fat
Number of LUNs=1
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
mousedev: PS/2 mouse device common for all mice
egalax_ts 1-0004: Failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: Failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2194000.usdhc: Got WP GPIO
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified
sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2198000.usdhc: Got WP GPIO
sdhci-esdhc-imx 2198000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@0219c000: voltage-ranges unspecified
sdhci-esdhc-imx 219c000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 219c000.usdhc: No vqmmc regulator found
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
usb 1-1: new high-speed USB device number 2 using ci_hdrc
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mxc_vpu 2040000.vpu_fsl: VPU initialized
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
wm8962 0-001a: Device is not a WM8962, ID 0 != 0x6243
wm8962: probe of 0-001a failed with error -22
imx-wm8962 sound: failed to find codec platform device
imx-wm8962: probe of sound failed with error -22
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Key type dns_resolver registered
mmc3: MAN_BKOPS_EN bit is not set
Registering SWP/SWPB emulation handler
input: gpio-keys as /devices/soc0/gpio-keys/input/input2
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
mmc3: new DDR MMC card at address 0001
mmcblk3: mmc3:0001 SEM08G 7.28 GiB
mmcblk3boot0: mmc3:0001 SEM08G partition 1 2.00 MiB
mipi_dsi_pwr_on: disabling
hdmi-5v-supply: disabling
sensor-supply: disabling
wm8962-supply: disabling
usb_h1_vbus: disabling
usb_otg_vbus: disabling
ALSA device list:
  No soundcards found.
Freeing unused kernel memory: 400K (80918000 - 8097c000)
mmcblk3boot1: mmc3:0001 SEM08G partition 2 2.00 MiB
mmcblk3rpmb: mmc3:0001 SEM08G partition 3 2.00 MiB
 mmcblk3: p1 p2
hub 1-1:1.0: USB hub found
hub 1-1:1.0: 4 ports detected
Starting UTP
uuc 0.5 [built Mar 12 2016 19:04:20]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0

///////

the progress blocked here...

 

 

Update:

 

Errors information as follow

 

"Push" error, file="D:\L4.1.15-1.0.0_ga-mfg-tools\mfgtools-with-rootfs\mfgtools\Profiles\linux\OS Firmware\mksdcard.sh.tar"

Original Attachment has been moved to: burnlog.txt.zip

Labels (3)
1 Solution
945 Views
liquanduan
Contributor III

Problem soloved....because U disk device is forbidden in my PC OS...i.mxSOLO board is recognized as a U disk device。

View solution in original post

3 Replies
946 Views
liquanduan
Contributor III

Problem soloved....because U disk device is forbidden in my PC OS...i.mxSOLO board is recognized as a U disk device。

945 Views
Yuri
NXP Employee
NXP Employee

Hello,

  from the following How to use Mfgtool with a Yocto i.MX6 build :

   mfgtool can use the same u-boot with the normal u-boot for our board. So we don’t need to build

the u-boot for mfgtool separately. So, try to build the U-boot as recommended in i.MX BSP Porting Guide.

Also :

Kernel configuration of zImage_mfgtool 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

945 Views
liquanduan
Contributor III

Thanks, Yuri,

so I think the problems might be not in building u-boot but configuring u-boot. According to the log info, the download stopped before partition storage device. I use eMMC in the hardware. Is there any id or address configuration settings for the storage device while building u-boot?

0 Kudos