Error while installing the extensible SDK on Ubuntu 18.04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error while installing the extensible SDK on Ubuntu 18.04

9,128 Views
thinhpham
Contributor I

Hello,

I have tried to build the extensible SDK but got an error that I have no idea what should I do to fix it. Note that with standard SDK, everything works well. Please help me!

ERROR: Task pseudo-native.do_fetch attempted to execute unexpectedly
<hashing...>
This is usually due to missing setscene tasks. Those missing in this build were: {'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-clang/recipes-devtools/clang/clang-cross_git.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-clang/recipes-devtools/clang/compiler-rt_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-clang/recipes-devtools/clang/libcxx_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-freescale-distro/recipes-fsl/fsl-rc-local/fsl-rc-local.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-freescale-distro/recipes-fsl/packagegroups/packagegroup-fsl-gstreamer1.0-full.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-freescale-distro/recipes-fsl/packagegroups/packagegroup-fsl-gstreamer1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-freescale-distro/recipes-fsl/packagegroups/packagegroup-fsl-tools-benchmark.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-freescale-distro/recipes-fsl/packagegroups/packagegroup-fsl-tools-gpu.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-freescale-distro/recipes-fsl/packagegroups/packagegroup-fsl-tools-testapps.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-freescale/recipes-bsp/imx-test/imx-test_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-freescale/recipes-core/udev/udev-rules-imx.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-bsp/firmware-imx/firmware-imx-8m_8.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-bsp/firmware-imx/firmware-imx_8.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-bsp/imx-atf/imx-atf_2.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-bsp/imx-kobs/imx-kobs_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-bsp/imx-mkimage/imx-boot_1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-bsp/imx-vpu-hantro/imx-vpu-hantro_1.20.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2020.04.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-connectivity/nxp-wlan-sdk/nxp-wlan-sdk_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-core/systemd/systemd-gpuconfig_1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-fsl/m4-demos/imx-m4-demos_2.8.0.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-graphics/drm/libdrm_2.4.102.imx.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-graphics/imx-gpu-apitrace/imx-gpu-apitrace_9.0.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-graphics/imx-gpu-viv/imx-gpu-viv_6.4.3.p1.0-aarch64.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-graphics/vulkan/assimp_5.0.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-graphics/wayland/wayland-protocols_1.20.imx.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-graphics/wayland/wayland_1.18.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-graphics/wayland/weston_9.0.0.imx.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-graphics/wayland/weston_9.0.0.imx.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-kernel/kernel-tests/kernel-pcitest.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-kernel/linux-libc-headers/linux-libc-headers_5.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx-headers_5.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb:do_shared_workdir',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-multimedia/alsa/imx-alsa-plugins_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-multimedia/gstreamer/imx-gst1.0-plugin_4.5.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-multimedia/imx-codec/imx-codec_4.5.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-multimedia/imx-dspc-asrc/imx-dspc-asrc_1.0.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-multimedia/imx-parser/imx-parser_4.5.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-multimedia/imx-sw-pdm/imx-sw-pdm_1.0.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-multimedia/imx-vpuwrap/imx-vpuwrap_4.5.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-security/optee-imx/optee-client_3.10.0.imx.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-security/optee-imx/optee-os_3.10.0.imx.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-security/optee-imx/optee-test_3.10.0.imx.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-security/smw/keyctl-caam_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-test/googletest/googletest_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-connectivity/sigma-dut/sigma-dut_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-connectivity/wireless-tools/wireless-tools_30.pre9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-devtools/half/half_2.1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-devtools/stb/stb_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-extended/jailhouse/jailhouse_0.12.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-extended/sudo/sudo_1.9.5p2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-fsl/images/imx-image-multimedia.bb:do_image_complete',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-fsl/images/imx-image-multimedia.bb:do_image_qa',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-fsl/images/imx-image-multimedia.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-fsl/images/imx-image-multimedia.bb:do_populate_lic',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-fsl/packagegroup/packagegroup-fsl-optee-imx.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-fsl/packagegroup/packagegroup-fsl-tools-audio.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-fsl/packagegroup/packagegroup-fsl-tools-gpu-external.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-fsl/packagegroup/packagegroup-imx-security.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/devil/devil_1.8.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/gli/gli_0.8.2.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/glm/glm_0.9.8.5.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/imx-gpu-sdk/imx-gpu-sdk_5.6.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/libgpuperfcnt/gputop_6.4.3.p1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/libgpuperfcnt/libgpuperfcnt_6.4.3.p1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/rapidopencl/rapidopencl_1.1.0.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/rapidopenvx/rapidopenvx_1.1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/rapidvulkan/rapidvulkan_1.2.141.2001.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/vulkan/glslang_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/vulkan/spirv-tools_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/vulkan/vkmark_1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/vulkan/vulkan-headers_1.1.121.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/vulkan/vulkan-loader_1.1.121.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/vulkan/vulkan-tools_1.1.121.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/vulkan/vulkan-validationlayers_1.1.121.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-multimedia/tinycompress/tinycompress_1.1.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-support/fmt/fmt_7.0.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-networking/recipes-connectivity/vlan/vlan_1.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-networking/recipes-daemons/ptpd/ptpd_2.3.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-networking/recipes-support/ntp/ntp_4.2.8p13.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-networking/recipes-support/ntp/ntp_4.2.8p13.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/bonnie/bonnie++_1.04.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/cpuburn/cpuburn-arm_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/dbench/dbench_4.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/fio/fio_3.16.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/glmark2/glmark2_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/iozone3/iozone3_484.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/iperf2/iperf2_2.0.13.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/iperf3/iperf3_3.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/lmbench/lmbench_3.0-a9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/memtester/memtester_4.3.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/nbench-byte/nbench-byte_2.2.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-benchmark/tiobench/tiobench_0.3.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-bsp/cpufrequtils/cpufrequtils_008.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-connectivity/hostapd/hostapd_2.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-connectivity/linuxptp/linuxptp_2.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-connectivity/packagegroups/packagegroup-tools-bluetooth.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-devtools/rapidjson/rapidjson_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-extended/socketcan/can-utils_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-extended/socketcan/libsocketcan_0.0.11.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-extended/tmux/tmux_2.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-security/keyutils/keyutils_1.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-support/fbset/fbset-modes.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-support/fbset/fbset_2.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-support/lvm2/lvm2_2.03.02.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-support/nano/nano_4.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-support/numactl/numactl_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-support/pps-tools/pps-tools_1.0.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-support/thin-provisioning-tools/thin-provisioning-tools_0.8.5.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-oe/recipes-test/evtest/evtest_1.34.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-python/recipes-devtools/python/python-pip_19.2.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-bsp/alsa-state/alsa-state.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-bsp/lrzsz/lrzsz_0.12.20.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-bsp/pciutils/pciutils_3.6.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-bsp/usbutils/usbutils_012.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/avahi/avahi_0.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/avahi/avahi_0.7.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/bluez5/bluez5_5.50.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/connman/connman-conf.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/connman/connman_1.37.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/iproute2/iproute2_5.2.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/iw/iw_5.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/libnss-mdns/libnss-mdns_0.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/libpcap/libpcap_1.9.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/mobile-broadband-provider-info/mobile-broadband-provider-info_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/neard/neard_0.16.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/nfs-utils/nfs-utils_2.4.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/nfs-utils/nfs-utils_2.4.1.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/ofono/ofono_1.30.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/openssl/openssl_1.1.1g.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/ppp/ppp_2.4.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/socat/socat_1.7.3.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-connectivity/wpa-supplicant/wpa-supplicant_2.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/base-files/base-files_3.0.14.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/base-passwd/base-passwd_3.5.29.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/busybox/busybox_1.31.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/coreutils/coreutils_8.31.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/dbus/dbus-test_1.12.16.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/dbus/dbus_1.12.16.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/dbus/dbus_1.12.16.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/dropbear/dropbear_2019.78.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/ell/ell_0.22.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/expat/expat_2.2.8.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/gettext/gettext_0.19.8.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/glib-2.0/glib-2.0_2.60.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/glib-networking/glib-networking_2.60.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/glibc/cross-localedef-native_2.30.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/glibc/glibc-locale_2.30.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/glibc/glibc-mtrace_2.30.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/glibc/glibc_2.30.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/glibc/ldconfig-native_2.12.1.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/initscripts/initscripts_1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/kbd/kbd_2.0.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/libxcrypt/libxcrypt_4.4.8.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/libxml/libxml2_2.9.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/ncurses/ncurses_6.1+20190803.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/netbase/netbase_5.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/os-release/os-release.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/packagegroups/packagegroup-base.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/packagegroups/packagegroup-core-boot.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/packagegroups/packagegroup-core-buildessential.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/packagegroups/packagegroup-core-nfs.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/packagegroups/packagegroup-core-sdk.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/packagegroups/packagegroup-core-ssh-dropbear.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/packagegroups/packagegroup-core-standalone-sdk-target.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/packagegroups/packagegroup-core-tools-debug.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/packagegroups/packagegroup-core-tools-profile.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/packagegroups/packagegroup-core-tools-testapps.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/psplash/psplash_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/readline/readline_8.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/systemd/systemd-compat-units.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/systemd/systemd-conf_243.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/systemd/systemd-serialgetty.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/systemd/systemd_243.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/systemd/systemd_243.2.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/udev/udev-extraconf_1.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/update-rc.d/update-rc.d_0.8.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/util-linux/util-linux_2.34.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/volatile-binds/volatile-binds.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/zlib/zlib_1.2.11.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/apt/apt-native_1.2.31.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/apt/apt_1.2.31.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/apt/apt_1.2.31.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/autoconf-archive/autoconf-archive_2019.01.06.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/autoconf/autoconf_2.69.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/automake/automake_1.16.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/binutils/binutils_2.32.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/bison/bison_3.4.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/btrfs-tools/btrfs-tools_5.2.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/ccache/ccache_3.7.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/diffstat/diffstat_1.62.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/dosfstools/dosfstools_4.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/dpkg/dpkg_1.19.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/e2fsprogs/e2fsprogs_1.45.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/elfutils/elfutils_0.177.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/expect/expect_5.45.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/file/file_5.37.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/flex/flex_2.6.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/gcc/gcc-runtime_9.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/gcc/gcc-sanitizers_9.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/gcc/gcc_9.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/gcc/libgcc_9.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/gdb/gdb-cross_8.3.1.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/gdb/gdb_8.3.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/gnu-config/gnu-config_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/i2c-tools/i2c-tools_4.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/intltool/intltool_0.51.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/json-c/json-c_0.13.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/libtool/libtool-cross_2.4.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/libtool/libtool_2.4.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/m4/m4_1.4.18.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/make/make_4.2.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/makedevs/makedevs_1.0.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/mklibs/mklibs-native_0.1.44.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/mmc/mmc-utils_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/mtd/mtd-utils_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/opkg-utils/opkg-utils_0.4.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/orc/orc_0.4.29.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/patch/patch_2.7.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/perl/libxml-parser-perl_2.44.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/perl/perl_5.30.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/pkgconfig/pkgconfig_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python-setuptools_41.2.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python3-dbus_1.2.12.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python3-mako_1.1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python3-pip_19.2.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python3-pycairo_1.18.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python3-pygobject_3.34.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python3-setuptools_41.2.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python3_3.7.8.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python_2.7.18.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/qemu/qemu-helper-native_1.0.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/qemu/qemu-system-native_4.1.0.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/qemu/qemuwrapper-cross_1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/quilt/quilt_0.66.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/run-postinsts/run-postinsts_1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/strace/strace_5.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/tcltk/tcl_8.6.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/valgrind/valgrind_3.15.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/at/at_3.1.23.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/bash/bash_5.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/bc/bc_1.07.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/blktool/blktool_4-7.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/bzip2/bzip2_1.0.8.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/cpio/cpio_2.12.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/cracklib/cracklib_2.9.5.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/cronie/cronie_1.5.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/cronie/cronie_1.5.4.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/diffutils/diffutils_3.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/ed/ed_1.15.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/ethtool/ethtool_5.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/findutils/findutils_4.6.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/gawk/gawk_5.0.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/grep/grep_3.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/gzip/gzip_1.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/iptables/iptables_1.8.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/iputils/iputils_s20190709.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/less/less_551.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/libaio/libaio_0.3.111.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/libidn/libidn2_2.2.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/libmnl/libmnl_1.0.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/libnsl/libnsl2_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/libtirpc/libtirpc_1.1.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/logrotate/logrotate_3.15.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/lsb/lsb-release_1.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/ltp/ltp_20190517.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/mc/mc_4.8.23.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/mdadm/mdadm_4.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/minicom/minicom_2.7.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/net-tools/net-tools_1.60-26.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/newt/libnewt_0.52.21.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/packagegroups/packagegroup-core-full-cmdline.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/pam/libpam_1.3.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/procps/procps_3.3.15.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/psmisc/psmisc_23.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/quota/quota_4.05.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/rpcbind/rpcbind_1.2.5.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/rpcbind/rpcbind_1.2.5.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/screen/screen_4.6.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/sed/sed_4.2.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/shadow/shadow-securetty_4.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/shadow/shadow-sysroot_4.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/shadow/shadow_4.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/slang/slang_2.3.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/sysklogd/sysklogd_1.5.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/tar/tar_1.32.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/tcp-wrappers/tcp-wrappers_7.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/time/time_1.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/timezone/tzcode-native.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/timezone/tzdata.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/unzip/unzip_6.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/which/which_2.21.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/xz/xz_5.2.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/zip/zip_3.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-gnome/gdk-pixbuf/gdk-pixbuf_2.38.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-gnome/gnome/adwaita-icon-theme_3.32.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-gnome/gobject-introspection/gobject-introspection_1.60.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-gnome/gtk+/gtk+3_3.24.8.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-gnome/hicolor-icon-theme/hicolor-icon-theme_0.17.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-gnome/json-glib/json-glib_1.4.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-gnome/libgudev/libgudev_233.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-gnome/librsvg/librsvg_2.40.20.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/cairo/cairo_1.16.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/cantarell-fonts/cantarell-fonts_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/clutter/clutter-1.0_1.26.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/cogl/cogl-1.0_1.22.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/fontconfig/fontconfig_2.13.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/freetype/freetype_2.10.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/harfbuzz/harfbuzz_2.6.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/jpeg/libjpeg-turbo_2.0.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/kmscube/kmscube_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/libepoxy/libepoxy_1.5.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/mesa/mesa_19.1.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/pango/pango_1.44.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/ttf-fonts/liberation-fonts_2.00.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/waffle/waffle_1.6.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/wayland/libinput_1.14.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/wayland/mtdev_1.1.5.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/wayland/weston-init.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libpciaccess_0.16.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libpthread-stubs_0.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libx11-compose-data_1.6.8.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxkbcommon_0.8.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/pixman_0.38.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/xkeyboard-config_2.27.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-proto/xorgproto_2019.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-util/util-macros_1.19.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/blktrace/blktrace_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/cryptodev/cryptodev-linux_1.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/cryptodev/cryptodev-module_1.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/cryptodev/cryptodev-tests_1.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/kern-tools/kern-tools-native_git.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/kexec/kexec-tools_2.0.19.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/kmod/kmod-native_git.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/kmod/kmod_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/linux-firmware/linux-firmware_20190815.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/lttng/babeltrace_1.5.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/lttng/lttng-modules_2.10.14.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/lttng/lttng-tools_2.10.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/lttng/lttng-tools_2.10.7.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/lttng/lttng-ust_2.10.5.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/make-mod-scripts/make-mod-scripts_1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/perf/perf.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/powertop/powertop_2.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/systemtap/systemtap_git.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/wireless-regdb/wireless-regdb_2020.04.29.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/alsa/alsa-lib_1.1.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/alsa/alsa-plugins_1.1.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/alsa/alsa-tools_1.1.7.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/alsa/alsa-utils_1.1.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/flac/flac_1.3.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.16.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.16.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-plugins-good_1.16.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-rtsp-server_1.16.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/gstreamer/gstreamer1.0_1.16.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/lame/lame_3.100.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/libogg/libogg_1.3.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/libpng/libpng_1.6.37.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/libsamplerate/libsamplerate0_0.1.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/libsndfile/libsndfile1_1.0.28.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/libtheora/libtheora_1.1.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/libtiff/tiff_4.0.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/libvorbis/libvorbis_1.3.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/mpg123/mpg123_1.25.11.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/pulseaudio/pulseaudio_12.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/pulseaudio/pulseaudio_12.2.bb:do_populate_sysroot',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/sbc/sbc_1.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/speex/speex_1.2.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/speex/speexdsp_1.2rc3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/webp/libwebp_1.0.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/atk/atk_2.32.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/attr/acl_2.2.52.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/attr/attr_2.4.47.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/bash-completion/bash-completion_2.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/boost/boost_1.71.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/ca-certificates/ca-certificates_20190110.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/curl/curl_7.66.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/db/db_5.3.28.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/debianutils/debianutils_4.8.6.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/fribidi/fribidi_1.0.5.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/gdbm/gdbm_1.18.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/gmp/gmp_6.1.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/gnome-desktop-testing/gnome-desktop-testing_2018.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/gnutls/gnutls_3.6.13.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/icu/icu_64.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/iso-codes/iso-codes_4.3.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libatomic-ops/libatomic-ops_7.6.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libcap-ng/libcap-ng_0.7.9.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libcap/libcap_2.27.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libcheck/libcheck_0.12.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libcroco/libcroco_0.6.13.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libdaemon/libdaemon_0.14.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libevdev/libevdev_1.8.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libevent/libevent_2.1.11.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libffi/libffi_3.3~rc0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libgcrypt/libgcrypt_1.8.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libgpg-error/libgpg-error_1.36.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libical/libical_3.0.6.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libmpc/libmpc_1.1.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libnl/libnl_3.5.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libpcre/libpcre_8.43.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libpsl/libpsl_0.21.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libsoup/libsoup-2.4_2.66.4.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libunistring/libunistring_0.9.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libunwind/libunwind_1.3.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/liburcu/liburcu_0.11.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libusb/libusb1_1.0.22.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/lzo/lzo_2.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/mpfr/mpfr_4.0.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/nettle/nettle_3.5.1.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/popt/popt_1.16.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/ptest-runner/ptest-runner_2.3.2.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/shared-mime-info/shared-mime-info_1.10.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/sqlite/sqlite3_3.29.0.bb:do_package',
'/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/taglib/taglib_1.11.1.bb:do_package',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-clang/recipes-devtools/clang/clang_git.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-devtools/python/python3-pycryptodomex_3.9.4.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-bsp/recipes-devtools/python/python3-pyelftools_0.25.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-imx/meta-sdk/recipes-graphics/vulkan/glslang_git.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/meta-openembedded/meta-python/recipes-devtools/python/python3-pycrypto_2.6.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-bsp/u-boot/u-boot-tools_2019.07.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/coreutils/coreutils_8.31.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/dbus/dbus_1.12.16.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-core/update-rc.d/update-rc.d_0.8.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/chrpath/chrpath_0.16.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/dosfstools/dosfstools_4.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/dpkg/dpkg_1.19.7.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/dwarfsrcfiles/dwarfsrcfiles.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/e2fsprogs/e2fsprogs_1.45.3.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/fdisk/gptfdisk_1.0.4.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/file/file_5.37.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/intltool/intltool_0.51.0.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/libedit/libedit_20190324-3.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/makedevs/makedevs_1.0.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/mtools/mtools_4.0.23.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/opkg-utils/opkg-utils_0.4.2.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/orc/orc_0.4.29.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/perl/libxml-parser-perl_2.44.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/perl/perl_5.30.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python-setuptools_41.2.0.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python3-mako_1.1.0.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/python/python3-six_1.12.0.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/rpm/rpm_4.14.2.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/swig/swig_3.0.12.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/tcltk/tcl_8.6.9.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/unfs3/unfs3_git.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/bc/bc_1.07.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/cwautomacros/cwautomacros_20110201.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/libarchive/libarchive_3.4.0.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/lzip/lzip_1.21.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/parted/parted_3.2.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/pbzip2/pbzip2_1.1.13.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/pigz/pigz_2.4.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/shadow/shadow_4.6.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-extended/zip/zip_3.0.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-gnome/gdk-pixbuf/gdk-pixbuf_2.38.2.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-gnome/gtk+/gtk+3_3.24.8.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-gnome/librsvg/librsvg_2.40.20.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/cairo/cairo_1.16.0.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/fontconfig/fontconfig_2.13.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/freetype/freetype_2.10.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/harfbuzz/harfbuzz_2.6.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/jpeg/libjpeg-turbo_2.0.3.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/libsdl2/libsdl2_2.0.10.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/pango/pango_1.44.6.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libice_1.0.10.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libpthread-stubs_0.4.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libsm_1.2.3.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libx11_1.6.8.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxau_1.0.9.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxcb_1.13.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxcomposite_0.4.5.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxcursor_1.2.0.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxdamage_1.1.5.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxdmcp_1.1.3.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxext_1.3.4.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxfixes_5.0.3.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxft_2.3.3.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxi_1.7.10.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxrandr_1.5.2.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxrender_0.9.10.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/libxtst_1.2.3.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/pixman_0.38.4.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-lib/xtrans_1.4.0.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-proto/xcb-proto_1.13.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-proto/xorgproto_2019.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-util/makedepend_1.0.6.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-graphics/xorg-util/util-macros_1.19.2.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-kernel/dtc/dtc_1.5.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/alsa/alsa-lib_1.1.9.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-multimedia/libpng/libpng_1.6.37.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/atk/at-spi2-atk_2.32.0.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/atk/at-spi2-core_2.32.1.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/atk/atk_2.32.0.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/bmap-tools/bmap-tools_3.5.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/debianutils/debianutils_4.8.6.3.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/fribidi/fribidi_1.0.5.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libcroco/libcroco_0.6.13.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/libxslt/libxslt_1.1.33.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/lzo/lzo_2.10.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/lzop/lzop_1.04.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/nspr/nspr_4.21.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/nss/nss_3.45.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/popt/popt_1.16.bb:do_populate_sysroot',
'virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-support/shared-mime-info/shared-mime-info_1.10.bb:do_populate_sysroot'}
ERROR: Task (virtual:native:/media/tpham/WORK/DevTools/yocto_esdk/layers/poky/meta/recipes-devtools/pseudo/pseudo_git.bb:do_fetch) failed with exit code 'setscene whitelist'

0 Kudos
Reply
11 Replies

9,110 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems that this is fetch the package error, try to delete this and build again

0 Kudos
Reply

9,107 Views
thinhpham
Contributor I

I tried to clone several versions of Zeus and build again but still got same problem. I even tried to create a clean Ubuntu and repeat all steps and no luck

0 Kudos
Reply

9,099 Views
joanxie
NXP TechSupport
NXP TechSupport

what's your build steps? pls send to me

 

0 Kudos
Reply

9,097 Views
thinhpham
Contributor I

Please check my steps:

1. With a clean Ubuntu 18.04.5 LTS, I installed all dependencies from https://community.nxp.com/t5/i-MX-Processors/Failed-to-build-yocto-for-imx8m-evk/m-p/1238640

2. Follow "5.6 Build scenarios" in https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf to build image for imx8mqevk

3. run `bitbake imx-image-multimedia -c populate_sdk_ext`

4. cd tmp/deploy/sdk and install ext sh installer

I encountered the error at step 4.

0 Kudos
Reply

9,085 Views
joanxie
NXP TechSupport
NXP TechSupport

for step 3, you run `bitbake imx-image-multimedia -c populate_sdk_ext` successfully, right?
 you failed on step4 install ext sh installer? how did you install the installer? what's your command? let me reproduce this

 

0 Kudos
Reply

9,071 Views
thinhpham
Contributor I

Yes, step 3 is success. For step 4, I cd to tmp/deploy/sdk, invoke the installer by ./fsl-imx-wayland-glibc-x86_64-imx-image-multimedia-aarch64-imx8mqevk-toolchain-ext-5.4-zeus.sh then see that error.

0 Kudos
Reply

9,031 Views
joanxie
NXP TechSupport
NXP TechSupport

did you try the other images? like imx-image-full? it seems this yocto version has issue with eSDK

 

 

0 Kudos
Reply

9,026 Views
thinhpham
Contributor I

I tried imx-image-full and core-image-sato but still no luck.

0 Kudos
Reply

9,023 Views
joanxie
NXP TechSupport
NXP TechSupport

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-build-U-Boot-Kernel-and-Linux-app...

refer to the document, did you copy the SDK to the host machine, then install and build it?

"

• From the build directory, the bitbake was run in, copy the sh file in tmp/deploy/sdk to the host machine to build on and execute the

script to install the SDK. The default location is in /opt but can be placed anywhere on the host machine.

"

 

0 Kudos
Reply

9,020 Views
thinhpham
Contributor I

I did not copy to anywhere. I have only one PC for building OS image, SDK and application development. Therefore, I just built the SDK, open it from tmp/deploy/sdk and install it to /opt/fsl-imx-wayland dir. I tried 2 cases with same process: on my PC and VM. The standard SDK was OK (I'm developing application on it) but extensible SDK was not.

0 Kudos
Reply

8,977 Views
joanxie
NXP TechSupport
NXP TechSupport

I have built different bsp version for eSDK, only mulitmeida image can be built successfully, but failed with full images, it seems that current bsp has issue about eSDK building

0 Kudos
Reply