Error while building iMX6 Platform SDK 1.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error while building iMX6 Platform SDK 1.1

6,067件の閲覧回数
letan
Contributor III

Hello together,

I have built i.MX6 Platform SDK 1.1 and encountered the issue as below when building with gcc-arm-embedded 4.9 (4.9-2015-q3-update : GCC ARM Embedded )

./tool/build_sdk

Building caam_blob_gen [mx6dq sabre_ai a]

make[1]: *** No rule to make target `/home/lia1hc/projects/iMX6_Platform_SDK/output/mx6dq/lib/libsdk.a', needed by `/home/lia1hc/projects/iMX6_Platform_SDK/output/mx6dq/caam_blob_gen/sabre_ai_rev_a/caam_blob_gen.elf'.  Stop.

make[1]: *** Waiting for unfinished jobs....

make: *** [caam_blob_gen] Error 2

Could you please help me on this?

Thanks,

Tan

ラベル(2)
タグ(1)
15 返答(返信)

5,519件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   please let me know Your e-mail or create NXP request (case) so, that I can send You

toolchain with SDK sources, that were tested. 

 
Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,519件の閲覧回数
Santhosha_rk
Contributor I

Hello Yuri,

Even I am looking for the link

My Email Id: santhosha.rk@accord-soft.com

Thanks,

Santhosha RK

0 件の賞賛
返信

5,519件の閲覧回数
Yuri
NXP Employee
NXP Employee

OK !

~Yuri.

0 件の賞賛
返信

5,519件の閲覧回数
Santhosha_rk
Contributor I

Thanks.

I would like to know one more information on the SDK.

Was camera test using OVP5642 working in SDK?

Regards,

Santhosha RK

0 件の賞賛
返信

5,519件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

ov5640 was tested with the SDP.

Regards,

Yuri.

0 件の賞賛
返信

5,519件の閲覧回数
Santhosha_rk
Contributor I

Thanks for the Quick Response.

We have configuration for Parallel video input. We need to test it using bare metal code. Will SDK work with the OV5642 if we change minimal code?

Will gigabit ethernet works in SDK? We are Planning to use Ping app. The used Phy is KSZ9021.

Regards,

Santhosha RK

0 件の賞賛
返信

5,519件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello.

Please look at my comments below.

1.

> Will SDK work with the OV5642 if we change minimal code?

  I think - yes ; basically the SDK has examples for both MIPI CSI-2 and

parallel CSI  interfaces.

2.

> Will gigabit ethernet works in SDK? We are Planning to use Ping app.

> The used Phy is KSZ9021

The loopback test does not work on the i.MX6 SDP/ SDB, but ping application

does work.

  Also the following helps.

"KSZ9031 on a SabreSD based board"

< https://community.freescale.com/message/504970 >

Regards,

Yuri.

5,519件の閲覧回数
letan
Contributor III

Hello Yuri,

My email is: lmtan91@gmail.com

I am looking forward you respond!

Thanks,

Tan

0 件の賞賛
返信

5,519件の閲覧回数
Yuri
NXP Employee
NXP Employee

done !

0 件の賞賛
返信

5,519件の閲覧回数
mcergun
Contributor III

Hi Yuri,

I am trying to open up a ticket to request a link to the Platform SDK but submit button doesn't work in any of my browsers. Can you please send me the link to the SDK, too?

Thanks,

Mert Can Ergun

mert-ergun@mikro-tasarim.com.tr

0 件の賞賛
返信

5,519件の閲覧回数
Yuri
NXP Employee
NXP Employee

  done !

Regards,

Yuri.

5,519件の閲覧回数
mcergun
Contributor III

thank you for the quick response Yuri.

but I don't have any emails containing the SDK, that may be due to my company e-mail limiting attachment size.

can you resend the email to mcergun90@gmail.com

0 件の賞賛
返信

5,519件の閲覧回数
Yuri
NXP Employee
NXP Employee

Done !

5,519件の閲覧回数
letan
Contributor III

Thank you so much

0 件の賞賛
返信

5,519件の閲覧回数
alancasinelli
Contributor II

Hello,

Could you please send me the same files too?

It seems the SDK has been removed from the download section of the site.

Edit: you should be able to find my e-mail in my profile, otherwise you can send at this address: *EDIT: removed*

Thank you.

0 件の賞賛
返信