Error when trying to build u-boot through Yocto project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error when trying to build u-boot through Yocto project

2,934件の閲覧回数
Ramprakash
Contributor II

Hi All,

I am trying to build u-boot from the yocto setup. I followed the steps mentioned in IMXLXYOCTOUG Rev. L5.4.70_2.3.0 — 31 December 2020 to setup the yocto project.

When i run the command  " $MACHINE=imx8qxpmek bitbake -c deploy u-boot-imx "

i get the following error "

ERROR: OE-core's config sanity checker detected a potential misconfiguration.
Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).
Following is the list of potential problems / advisories:

MACHINE=imx8qxpmek is invalid. Please set a valid MACHINE in your local.conf, environment or other configuration file.

"

I am using a Ubuntu 16.04 machine. How to fix this issue?

Thanks and Regards,

Ramprakash

0 件の賞賛
返信
2 返答(返信)

2,928件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the yocto user guide, The recommended minimum Ubuntu version is 18.04 or later

0 件の賞賛
返信

2,916件の閲覧回数
Ramprakash
Contributor II

Hi @joanxie ,

Yes, I did go through the yocto guide and I saw ubuntu 16.04 LTS are one of the build system. Anyway I'll try again with Ubuntu 18.04 LTS.

Thanks and Regards,

Ramprakash

0 件の賞賛
返信