Error reading cluster for SD card boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error reading cluster for SD card boot

3,459件の閲覧回数
t2865k5
Contributor I

Dear NXP ,

 

U-Boot version : 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)

HW platform: srg-imx8mplus (base on imx8mplus)

Memory : MT53D512M32D2 (2GB)

SD card : SP 16GB and SanDisk 16GB

 

Build a bootable SD card for imx8mplus platform . Use the SD card to boot in srg-imx8mplus platform .

In Uboot mode , this message is as follows:

switch to partitions #0, OK
mmc1 is current device
Error reading cluster

 

It can't boot normally form SD card. Please help to fix this issue.

 

t2865k5_0-1657000929742.png

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,441件の閲覧回数
t2865k5
Contributor I

Dear NXP ,

This issue needs to be resolved as soon as possible. I have been waiting for a very long time ,and I hope you can help us resolve this issue.

0 件の賞賛
返信

3,071件の閲覧回数
www1519
Contributor III

Dear  t2865k5

Has the problem been solved? What countermeasures is it.

The same trouble has happened. 

0 件の賞賛
返信