Dear Sir:
I compile and use caam according to the link https://community.nxp.com/docs/DOC-343823 .The system compiled by the provided method cannot run on the official imx8qxpmek board .while boot , show below error (attachment picture 1)
Then I replaced it with a kernel compiled by myself, that can run, but the test program has an error:(attachment picture 2)
After starting, load the cryptodev driver and run cv2x_benchmark. The software operation part at the beginning is no problem. The hardware part that uses CAAM to accelerate the operation reports an error and crashes.
It was compiled using the method he last updated on October 14.(attachment picture 3)
Hope for your response asap , thanks.i.MX Processors
Which version of Yocto release you used? Do you use a clean code base to build meta-cv2x instead of existed build folder?
Hi Xiaodong:
非常感谢回复!yocto的版本和帖子里的保持了一致:
Linux kernel: imx_4.14.98_2.0.0_ga
其他操作步骤也是严格按照帖子里的步骤来操作的:
Linux kernel: imx_4.14.98_2.0.0_ga
cryptodev: 1.9
HW platform: i.MX8M/MM/MN, i.MX8QM/QXP.
How to build:
1, decompress meta-cv2x_4.14.98_2.0.0_ga.tgz and copy meta-cv2x to folder (Yocto 4.14.98_2.0.0_ga dir)/sources/
2, Run DISTRO=fsl-imx-wayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build-cv2x and add BBLAYERS += " $/sources/meta-cv2x " into (Yocto 4.14.98_2.0.0_ga dir)/build-cv2x/conf/bblayers.conf and IMAGE_INSTALL_append += " gmssl-bin " into local.conf
3, Run bitbake fsl-image-validation-imx.
4, You can find cv2x-verify.c under (build dir)/tmp/work/aarch64-poky-linux/cryptodev-tests/1.9-r0/git/tests. It is example for using CAAM cryptdev interface to do C-V2X verification (includes SM2 p256, NIST p256 and brainpoolP256r1). cv2x_benchmark.c under (build dir)/tmp/work/aarch64-poky-linux/gmssl/1.0-r0/gmssl-1.0/test is the benchmark test program of C-V2X verifying. It includes HW, SW and HW+SW(one CPU) verifying for SM2 p256, NIST p256 and brainpoolP256r1.
5, Run the below command on your i.MX8QXP MEK board.
modprobe cryptodev
./cv2x_benchmark
谢谢!
Best Regards
Can you try to run "gmssl speed sm2" after command "modprobe cryptodev"?