Error kernel-module-nxp89xx: do_compile for changing DEBUG LEVEL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error kernel-module-nxp89xx: do_compile for changing DEBUG LEVEL

1,550 次查看
tanoue
Contributor III

Hi,

How kernel-module-nxp89xx's debug output to be disabled?

 

I would like to my image for i.MX8M Plus based on NXP BSP(Linux 5.15.32_2.0.0).

When I use Wi-Fi, the following command is needed to load Wi-Fi driver(moal.ko, mlan.ko).

modprobe moal mod_para=nxp/wifi_mod_para.conf

However, moal and mlan keep giving debug output after modprobe command like that.

[   35.991569] wlan: wfd0 START SCAN
[   40.337134] wlan: SCAN COMPLETED: scanned AP count=41
[   40.345986] wlan: sched scan start

So, I tried to patch Makefile to changing DEBUG LEVEL.

But compile error occured.

/home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_shim.c: In function 'moal_get_hw_spec_complete':
/home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_shim.c:875:15: warning: unused variable 'drv_mode' [-Wunused-variable]
875 | t_u32 drv_mode = handle->params.drv_mode;
| ^~~~~~~~
/home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_shim.c: In function 'moal_recv_event':
/home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_shim.c:2854:21: error: 'drvdbg' undeclared (first use in this function); did you mean 'dev_dbg'?
2854 | if (drvdbg & MFW_D)
| ^~~~~~
| dev_dbg
/home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_shim.c:2854:21: note: each undeclared identifier is reported only once for each function it appears in
/home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_shim.c:2854:30: error: 'MFW_D' undeclared (first use in this function)
2854 | if (drvdbg & MFW_D)
| ^~~~~
CC [M] /home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_uap_cfg80211.o
/home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_main.c: In function 'woal_tx_timeout':
/home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_main.c:6180:21: error: 'drvdbg' undeclared (first use in this function); did you mean 'dev_dbg'?
6180 | if (drvdbg & MFW_D)
| ^~~~~~
| dev_dbg
/home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_main.c:6180:21: note: each undeclared identifier is reported only once for each function it appears in
make[1]: *** [/home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source/scripts/Makefile.build:277: /home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_shim.o] Error 1
make[1]: *** Waiting for unfinished jobs....
/home/feadmin/work/imx-yocto-bsp/build-xwayland-kirkstone/tmp/work/imx8mp_lpddr4_evk-poky-linux/kernel-module-nxp89xx/1.0-r0/git/mxm_wifiex/wlan_src/mlinux/moal_main.c:6180:30: error: 'MFW_D' undeclared (first use in this function)
6180 | if (drvdbg & MFW_D)
| ^~~~~

How to solve it?

 

Patch file, bb file and build logs are attached.

 

Best Regard.

Tanoue.

 

 

 

0 项奖励
回复
2 回复数

1,533 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The CONFIG_DEBUG max value that makefile support is 2. Please modify this value in your patch.

ifeq ($(CONFIG_DEBUG),1)
	ccflags-y += -DDEBUG_LEVEL1
endif

ifeq ($(CONFIG_DEBUG),2)
	ccflags-y += -DDEBUG_LEVEL1
	ccflags-y += -DDEBUG_LEVEL2
	DBG=	-dbg
endif

 

0 项奖励
回复

1,528 次查看
tanoue
Contributor III

Hi, @Zhiming_Liu .

 

Thank you for reply.

I already knew CONFIG_DEBUG's max value is 2.

What I am referring to is that CONFIG_DEBUG supports n(none) according to comments in Makefile, but the source code does not.

 

Comments is here

# Debug Option
# DEBUG LEVEL n/1/2:
# n: NO DEBUG
# 1: Only PRINTM(MMSG,...), PRINTM(MFATAL,...), ...
# 2: All PRINTM()
CONFIG_DEBUG=1
 
I think patching the Makefile is not enough, what do you think?
 
Best Regards.
Tanoue.
0 项奖励
回复