Error in ipu unit test on 3.14.28 kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in ipu unit test on 3.14.28 kernel

516 Views
chaitanyadhere
Contributor I

Hello,

          I am using the freescale linux 3.14.28 kernel on a custom IMX6Q based board. I am getting an issue when I run the autorun-ipu.sh. The log is as follows:

imx-ipuv3 2400000.ipu: mxc ipu: unimplemented pixel format

What can be the issue ? Is there anything missing during initialization ?

Thanks,

Chaitanya Dhere

0 Kudos
1 Reply

407 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Perhaps You need to build GUI or QT5 version.

I tried the ipu test under L3.14.38 and did not detected the mentioned message.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos