Hello All,
I added packages "libav" and "ffmpeg" in sources/recipies-fsl/images/fsl-image-multimedia.bb but i got the logs as seen below. multimedia images doesn't support this kind of audio/video codec or vice versa. But the same error was found for core-image-minimal as well. Can anyone help me in this?
######################################################################################################################################################################################################################################
manju@manju-ThinkCentre-A85:~/projects/yocto/fsl-community-bsp/build$ bitbake fsl-image-multimedia
Loading cache: 100% |###########################################| ETA: 00:00:00
Loaded 2078 entries from dependency cache.
Parsing recipes: 100% |#########################################| Time: 00:00:00
Parsing of 1621 .bb files complete (1619 cached, 2 parsed). 2077 targets, 127 skipped, 0 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'libav' (but /home/manju/projects/yocto/fsl-community-bsp/sources/meta-pga/recipes-fsl/images/fsl-image-multimedia.bb RDEPENDS on or otherwise requires it)
ERROR: libav was skipped: because it has a restricted license not whitelisted in LICENSE_FLAGS_WHITELIST
ERROR: libav was skipped: because it has a restricted license not whitelisted in LICENSE_FLAGS_WHITELIST
NOTE: Runtime target 'libav' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['libav']
ERROR: Required build target 'fsl-image-multimedia' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-multimedia', 'libav']
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
#######################################################################################################################################################################################################################################
Which image is most suited for libav or ffmpeg?
Regards,
Manju
Solved! Go to Solution.
Thank you for replying. I could build Yocto with "libav" but not "ffmpeg".
any error message for "ffmpeg"?
manju@manju-ThinkCentre-A85:~/projects/yocto/fsl-community-bsp/build$ bitbake fsl-image-multimedia
Loading cache: 100% |########################################################################################################################################################################| ETA: 00:00:00
Loaded 2078 entries from dependency cache.
Parsing recipes: 100% |######################################################################################################################################################################| Time: 00:00:00
Parsing of 1621 .bb files complete (1619 cached, 2 parsed). 2077 targets, 106 skipped, 0 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'ffmpeg' (but /home/manju/projects/yocto/fsl-community-bsp/sources/meta-pga/recipes-fsl/images/fsl-image-multimedia.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target 'ffmpeg' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['ffmpeg']
ERROR: Required build target 'fsl-image-multimedia' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-multimedia', 'ffmpeg']
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
I think there may something wrong in the bb file. could you show the bb file?
DESCRIPTION = "A console-only image that includes gstreamer packages and \
Freescale's multimedia packages (VPU and GPU) when available for the specific \
machine."
IMAGE_FEATURES += "\
${@base_contains('DISTRO_FEATURES', 'x11', 'x11-base', '', d)} \
"
LICENSE = "MIT"
inherit core-image
CORE_IMAGE_EXTRA_INSTALL += " \
# (qt multimedia related other packages here) \
ffmpeg \
"
Thanks a lot jimmychan