Error in SRK table key generated from IMX_CST_TOOL_NEW

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error in SRK table key generated from IMX_CST_TOOL_NEW

3,246 次查看
KiranM7
Contributor I

    I want to implement Secure Boot on FRDM i.MX 91 Development Board. So far I have generated Private & Public Keys by following - https://wiki.amarulasolutions.com/opensource/uboot/secure_boot/imx8mm_habv4.html
and using IMX_CST_TOOL_NEW. I am referring https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf to set a Yocto build for code signing. I have followed these steps 

1. 
repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-styhead -m
imx-6.12.3-1.0.0_security-reference-design.xml
repo sync
MACHINE=imx91-11x11-lpddr4-evk DISTRO=fsl-imx-xwayland source imx-setup-release.sh -b frdm-imx91
2. Add the meta-secure-boot layer to the Yocto project.
bitbake-layers add-layer ../sources/meta-nxp-security-reference-design/meta-
secure-boot
3. Add CST or SPSDK in SIG_TOOL_PATH in local.conf.
echo "SIG_TOOL_PATH = \"/home/Kiran/Downloads/IMX_CST_TOOL_NEW/cst-4.0.0\"" >> conf/local.conf

To generate a signed bootloader/kernel/WIC image in Yocto project:
Build a signed WIC image.
bitbake core-image-minimal-secure-boot
On running the above command I get below error
.....
meta-secure-boot     = "HEAD:8f8264146cb639a6eee13da463560c5e7a893fb2"

Sstate summary: Wanted 22 Local 6 Mirrors 0 Missed 16 Current 2516 (27% match, 99% complete)####         | ETA:  0:00:00
Initialising tasks: 100% |###############################################################################| Time: 0:00:01
NOTE: Executing Tasks
ERROR: imx-boot-signature-1.0-r0 do_compile: Execution of '/home/Kiran/SEC_YOCTO/frdm-imx91/tmp/work/imx91_11x11_lpddr4_evk-poky-linux/imx-boot-signature/1.0/temp/run.do_compile.88482' failed with exit code 255
ERROR: Logfile of failure stored in: /home/Kiran/SEC_YOCTO/frdm-imx91/tmp/work/imx91_11x11_lpddr4_evk-poky-linux/imx-boot-signature/1.0/temp/log.do_compile.88482
Log data follows:
 DEBUG: Executing shell function do_compile
 NOTE: Signing boot image
Install SRK
Super Root Key table is invalid in file File/home/Kiran/cst/IMX_CST_TOOL_NEW/cst-4.0.0/crts/SRK_1_2_3_4_table.bin in command InstallSRK
ERROR: Failed to sign the image using: container_2.csf
imx_signer.c:main:1959: SIG_TOOL_PATH set to: "/home/Kiran/cst/IMX_CST_TOOL_NEW/cst-4.0.0"
imx_signer.c:main:1960: SIG_DATA_PATH set to: "/home/Kiran/cst/IMX_CST_TOOL_NEW/cst-4.0.0"
imx_signer.c:main:1961: Input filename = imx-boot-imx91-11x11-lpddr4-evk-sd.bin-flash_singleboot
imx_signer.c:main:1962: Output filename = signed-imx-boot-imx91-11x11-lpddr4-evk-sd.bin-flash_singleboot
imx_signer.c:main:1964: Input CSF Configuration filename = /home/Kiran/SEC_YOCTO/frdm-imx91/tmp/work/imx91_11x11_lpddr4_evk-poky-linux/imx-boot-signature/1.0/imx-boot-signature-1.0/sign.cfg
imx_signer.c:main:1974: Input filesize = 2032640 bytes
imx_signer.c:main:1988: IVT header = TAG:0x87 | LEN:0x0220 | VER:0x00
imx_signer.c:sign_container:963: Image Flag type: 0x6
imx_signer.c:sign_container:969: Container 0 already signed
imx_signer.c:sign_container:972: file_off = 0x00000400
imx_signer.c:sign_container:963: Image Flag type: 0x3
imx_signer.c:sign_container:987: file_off = 0x00000800 imx_signer.c:sign_container:996: APP container offset = 0x00049800
imx_signer.c:sign_container:997: APP container signature offset = 0x00049990
imx_signer.c:sign_container:1009: CSF Container:	 Container Number : 0
imx_signer.c:sign_container:1010: Container Offset : 0x00000000
imx_signer.c:sign_container:1011: Signature Offset : 0x00000000
imx_signer.c:sign_container:1009: CSF Container:	 Container Number : 2
imx_signer.c:sign_container:1010: Container Offset : 0x00000400
imx_signer.c:sign_container:1011: Signature Offset : 0x00000490
imx_signer.c:sign_container:1009: CSF Container:	 Container Number : 3
imx_signer.c:sign_container:1010: Container Offset : 0x00049800
imx_signer.c:sign_container:1011: Signature Offset : 0x00049990
imx_signer.c:sign_container:1009: CSF Container:	 Container Number : 0
imx_signer.c:sign_container:1010: Container Offset : 0x00000000
imx_signer.c:sign_container:1011: Signature Offset : 0x00000000
imx_signer.c:sign_container:1044: CSF filename = container_2.csf
INFO: container_2.csf generated
imx_signer.c:sign_container:1051: CSF filename created = container_2.csf
Executing command: /home/Kiran/cst/IMX_CST_TOOL_NEW/cst-4.0.0/linux64/bin/cst --verbose --i container_2.csf --o otemp.bin
| WARNING: exit code 255 from a shell command.
ERROR: Task (/home/Kiran/SEC_YOCTO/sources/meta-nxp-security-reference-design/meta-secure-boot/recipes-secure-boot/imx-mkimage/imx-boot-signature.bb:do_compile) failed with exit code '1'
ERROR: linux-imx-signature-1.0-r0 do_compile: Execution of '/home/Kiran/SEC_YOCTO/frdm-imx91/tmp/work/imx91_11x11_lpddr4_evk-poky-linux/linux-imx-signature/1.0/temp/run.do_compile.88485' failed with exit code 255
ERROR: Logfile of failure stored in: /home/Kiran/SEC_YOCTO/frdm-imx91/tmp/work/imx91_11x11_lpddr4_evk-poky-linux/linux-imx-signature/1.0/temp/log.do_compile.88485
Log data follows:
DEBUG: Executing shell function do_compile
NOTE: Signing kernel image
Install SRK
Super Root Key table is invalid in file File/home/Kiran/cst/IMX_CST_TOOL_NEW/cst-4.0.0/crts/SRK_1_2_3_4_table.bin in command InstallSRK
ERROR: Failed to sign the image using: container_1.csf
imx_signer.c:main:1959: SIG_TOOL_PATH set to: "/home/Kiran/cst/IMX_CST_TOOL_NEW/cst-4.0.0"
imx_signer.c:main:1960: SIG_DATA_PATH set to: "/home/Kiran/cst/IMX_CST_TOOL_NEW/cst-4.0.0"
imx_signer.c:main:1961: Input filename = flash_os.bin
imx_signer.c:main:1962: Output filename = signed-flash_os.bin
imx_signer.c:main:1964: Input CSF Configuration filename = /home/Kiran/SEC_YOCTO/frdm-imx91/tmp/work/imx91_11x11_lpddr4_evk-poky-linux/linux-imx-signature/1.0/linux-imx-signature-1.0/sign.cfg
imx_signer.c:main:1974: Input filesize = 35030016 bytes
imx_signer.c:main:1988: IVT header = TAG:0x87 | LEN:0x0120 | VER:0x00
imx_signer.c:sign_container:963: Image Flag type: 0x3
imx_signer.c:sign_container:987: file_off = 0x00000400
imx_signer.c:sign_container:1009: CSF Container:	 Container Number : 1
imx_signer.c:sign_container:1010: Container Offset : 0x00000000
imx_signer.c:sign_container:1011: Signature Offset : 0x00000110
imx_signer.c:sign_container:1009: CSF Container:	 Container Number : 0
imx_signer.c:sign_container:1010: Container Offset : 0x00000000
imx_signer.c:sign_container:1011: Signature Offset : 0x00000000
imx_signer.c:sign_container:1009: CSF Container:	 Container Number : 0
imx_signer.c:sign_container:1010: Container Offset : 0x00000000
imx_signer.c:sign_container:1011: Signature Offset : 0x00000000
imx_signer.c:sign_container:1009: CSF Container:	 Container Number : 0
imx_signer.c:sign_container:1010: Container Offset : 0x00000000
imx_signer.c:sign_container:1011: Signature Offset : 0x00000000
imx_signer.c:sign_container:1044: CSF filename = container_1.csf
INFO: container_1.csf generated
imx_signer.c:sign_container:1051: CSF filename created = container_1.csf
Executing command: /home/Kiran/cst/IMX_CST_TOOL_NEW/cst-4.0.0/linux64/bin/cst --verbose --i container_1.csf --o signed-flash_os.bin
WARNING: exit code 255 from a shell command.
ERROR: Task (/home/Kiran/SEC_YOCTO/sources/meta-nxp-security-reference-design/meta-secure-boot/recipes-secure-boot/linux/linux-imx-signature.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 5207 tasks of which 5203 didn't need to be rerun and 2 failed.

Summary: 2 tasks failed:
  /home/Kiran/SEC_YOCTO/sources/meta-nxp-security-reference-design/meta-secure-boot/recipes-secure-boot/imx-mkimage/imx-boot-signature.bb:do_compile
    log: /home/Kiran/SEC_YOCTO/frdm-imx91/tmp/work/imx91_11x11_lpddr4_evk-poky-linux/imx-boot-signature/1.0/temp/log.do_compile.88482
  /home/Kiran/SEC_YOCTO/sources/meta-nxp-security-reference-design/meta-secure-boot/recipes-secure-boot/linux/linux-imx-signature.bb:do_compile
    log: /home/Kiran/SEC_YOCTO/frdm-imx91/tmp/work/imx91_11x11_lpddr4_evk-poky-linux/linux-imx-signature/1.0/temp/log.do_compile.88485
Summary: There were 2 ERROR messages, returning a non-zero exit code.

 

The error snap from above code: 

Super Root Key table is invalid in file File/home/Kiran/cst/IMX_CST_TOOL_NEW/cst-4.0.0/crts/SRK_1_2_3_4_table.bin in command InstallSRK
ERROR: Failed to sign the image using: container_2.csf
imx_signer.c:main:1959: SIG_TOOL_PATH set to: 

I have followed these steps to generate the SRK keys

$ echo "42424242" > serial

$ echo "Amarual357" > key_pass.txt
$ echo "Amarual357" >> key_pass.txt
$ ./hab4_pki_tree

Do you want to use an existing CA key (y/n)?: n

Key type options (confirm targeted device supports desired key type):
Select the key type (possible values: rsa, rsa-pss, ecc)?: rsa
Enter key length in bits for PKI tree: 2048
Enter PKI tree duration (years): 10
How many Super Root Keys should be generated? 4
Do you want the SRK certificates to have the CA flag set? (y/n)?: y

 

Kiran@LinuxNew:~/cst/IMX_CST_TOOL_NEW/cst-4.0.0/crts$ ../linux64/bin/srktool -h 4 -t SRK_1_2_3_4_table.bin -e SRK_1_2_3_4_fuse.bin -d sha256 -c ./SRK1_sha256_2048_65537_v3_ca_crt.pem,./SRK2_sha256_2048_65537_v3_ca_crt.pem,./SRK3_sha256_2048_65537_v3_ca_crt.pem,./SRK4_sha256_2048_65537_v3_ca_crt.pem
Number of certificates = 4
SRK table binary filename = SRK_1_2_3_4_table.bin
SRK Fuse binary filename = SRK_1_2_3_4_fuse.bin
SRK Fuse binary dump:
SRKH[0] = 0x542C6295
SRKH[1] = 0x41D0DB63
SRKH[2] = 0x96D4FB34
SRKH[3] = 0x2FE8944E
SRKH[4] = 0xEF82C54D
SRKH[5] = 0xC956909F
SRKH[6] = 0xA5A5365D
SRKH[7] = 0x33E50E18

The Yocto build is failing because of invalid SRK_1_2_3_4_table.bin. 

Please help in resolving this issue for i.MX91 processor. 

Also, let me know if I have to follow some specific guide for getting a signed image through IMX_CST_TOOL_NEW - cst-4.0.0 tool.

0 项奖励
回复
17 回复数

3,199 次查看
KiranM7
Contributor I

Hi,

Requesting you to provide help with respect to NXP Code Signing Tool to get the correct SRK_Table.bin generated from iMX91 processor point of view. I know there is no support for FRDM iMX91 dev board, but at least give some guidance on how to do it for iMX 91 processor.

Thx,

Kiran.  

0 项奖励
回复

3,146 次查看
Harvey021
NXP TechSupport
NXP TechSupport

To set "n" for the "Do you want the SRK certificates to have the CA flag set? (y/n)?: y"

and the UG10195 to build image for FRDM.

 

Regards

Harvey

 

0 项奖励
回复

3,122 次查看
KiranM7
Contributor I

Hi,

    Even after setting 'n' option for "Do you want the SRK certificates to have the CA flag set? (y/n)?:n" the SRK_1_2_3_4_table.bin is still recognised as invalid file. Kindly help.

Thx,

Kiran.

 

0 项奖励
回复

3,084 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Chage the key type to rsa-pss or ecc.

 

Regards

Harvey

0 项奖励
回复

3,056 次查看
KiranM7
Contributor I

Hi,

    I changed the key type to ECC. Executed below commands to generate the key:

Do you want to use an existing CA key (y/n)?: n

Key type options (confirm targeted device supports desired key type):
Select the key type (possible values: rsa, rsa-pss, ecc)?: ecc
Enter length for elliptic curve to be used for PKI tree:
Possible values p256, p384, p521: p256
Enter the digest algorithm to use: sha256
Enter PKI tree duration (years): 10
Do you want the SRK certificates to have the CA flag set? (y/n)?: y

After the keys were generated renamed secp256r1 with prime256v1, this ensured the Yocto build went ahead and was successful albiet with setting MACHINE= imx91-11x11-lpddr4-evk.  

I have this image core-image-minimal-secure-boot-imx91-11x11-lpddr4-evk.rootfs-20250625112623.wic.zst ready now.

So far I have executed following bitbake commands:

bitbake core-image-minimal-secure-boot

bitbake imx-boot-signature

bitbake linux-imx-signature

Can you please suggest the next steps in verifying that the secure boot works.

0 项奖励
回复

3,042 次查看
Harvey021
NXP TechSupport
NXP TechSupport

We recommend to run the "ahab_status" in U-Boot to verify that secure boot work. 

For more information on how to program the SRK Fuses, verifying signature and closing
the part to enable secure boot, see the secure boot user guide, - ahab_guide 

As you're working with FRDM board. To Integrate the i.MX FRDM layer to BSP is needed. UG10195 

As previous post about secure boot for FRMD board, R&D will have a plan for that in the late of this year. 

 

Regards

Harvey

0 项奖励
回复

2,934 次查看
KiranM7
Contributor I

Hi,

Today I flashed the core-image-base-imx91-11x11-lpddr4-evk.rootfs.wic.zst onto the iMX-FRDM board and got below log on u-boot, can you please suggest the things that I am missing.

Retry time exceeded; starting again

Authenticate OS container at 0x98000000

Error: Wrong container header

ERR: failed to authenticate

u-boot=> aha_status

Lifecycle: 0x00000008, OEM Open

        0x0287eed6

        IPC = MU APD (0x2)

        CMD = ELE_OEM_CNTN_AUTH_REQ (0x87)

        IND = ELE_NO_AUTHENTICATION_FAILURE_IND (0xEE)

        STA = ELE_SUCCESS_IND (0xD6) 

        0x0287eed6

        IPC = MU APD (0x2)

        CMD = ELE_OEM_CNTN_AUTH_REQ (0x87)

        IND = ELE_NO_AUTHENTICATION_FAILURE_IND (0xEE)

        STA = ELE_SUCCESS_IND (0xD6)

 

0 项奖励
回复

2,914 次查看
Harvey021
NXP TechSupport
NXP TechSupport

The <IND = ELE_NO_AUTHENTICATION_FAILURE_IND (0xEE)> is an indication of that not signed. 

Regards

Harvey

0 项奖励
回复

2,876 次查看
KiranM7
Contributor I

Hi, today I flashed signed-imx-boot-imx91-11x11-lpddr4-evk-sd.bin-flash_singleboot and it's still stuck up in u-boot, please find the snap below:

Retry time exceeded; starting again
Authenticate OS container at 0x98000000
Error: Wrong container header
ERR: failed to authenticate
u-boot=> ahab_status
Lifecycle: 0x00000008, OEM Open


        0x0287fad6
        IPC = MU APD (0x2)
        CMD = ELE_OEM_CNTN_AUTH_REQ (0x87)
        IND = ELE_BAD_KEY_HASH_FAILURE_IND (0xFA)
        STA = ELE_SUCCESS_IND (0xD6)

        0x0287fad6
        IPC = MU APD (0x2)
        CMD = ELE_OEM_CNTN_AUTH_REQ (0x87)
        IND = ELE_BAD_KEY_HASH_FAILURE_IND (0xFA)
        STA = ELE_SUCCESS_IND (0xD6)
u-boot=> %   
0 项奖励
回复

2,847 次查看
Harvey021
NXP TechSupport
NXP TechSupport

The IND = ELE_BAD_KEY_HASH_FAILURE_IND (0xFA) 

Key does not match with the OTP that SRK hashes fused on the target, or the event can be displayed in case the SRK fuses are not programmed yet.

 

Regards

Harvey 

0 项奖励
回复

2,806 次查看
KiranM7
Contributor I

Hi,

After flashing the 2 files:

1. core-image-minimal-secure-boot-imx91-11x11-lpddr4-evk.rootfs.wic.zst

2. signed-imx-boot-imx91-11x11-lpddr4-evk-sd.bin-flash_singleboot

When I check ahab_status on u-boot I get the below message and also the board boots completely till Linux

Hit any key to stop autoboot:  0
u-boot=>
u-boot=> ahab_status
Lifecycle: 0x00000008, OEM Open
        0x0287eed6
        IPC = MU APD (0x2)
        CMD = ELE_OEM_CNTN_AUTH_REQ (0x87)
        IND = ELE_NO_AUTHENTICATION_FAILURE_IND (0xEE)
        STA = ELE_SUCCESS_IND (0xD6)
        0x0287eed6
        IPC = MU APD (0x2)
        CMD = ELE_OEM_CNTN_AUTH_REQ (0x87)
        IND = ELE_NO_AUTHENTICATION_FAILURE_IND (0xEE)
        STA = ELE_SUCCESS_IND (0xD6)
u-boot=>

 

Please let me know if this indicates that the secure boot is working correctly. Also, how can I test this by trying corresponding non-secure image? 

NOTE: I haven't yet flashed the fuses. I wan't to check whether the secure boot works without flashing the fuses first. Once this step is completed then I will flash the fuses.

Thx,

Kiran. 

 

0 项奖励
回复

2,789 次查看
Harvey021
NXP TechSupport
NXP TechSupport

SRK fuse is the basis of root of trust, to power on the board and run ahab_status command on U-Boot terminal is recommended method. 

For details, please refer to the ahab and AN12312 

 

Regards

Harvey

0 项奖励
回复

2,778 次查看
KiranM7
Contributor I

Hi,

Can I use fuse override option to test secure boot, without flashing the actual fuses? Can you please help with examples if applicable?

Thx,

Kiran.

0 项奖励
回复

2,771 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Considering the security requirements, there is no shadow related to the override function in SRK Fuse. Otherwise, it will lead to security risks.

 

Regards

Harvey

0 项奖励
回复

2,754 次查看
KiranM7
Contributor I

Hi,

I have generated below keys through NXP CST:

 

Do you want to use an existing CA key (y/n)?: n

Key type options (confirm targeted device supports desired key type):

Select the key type (possible values: rsa, rsa-pss, ecc)?: ecc

Enter length for elliptic curve to be used for PKI tree:

Possible values p256, p384, p521:  p384

Enter the digest algorithm to use: sha384

Enter PKI tree duration (years): 5

Do you want the SRK certificates to have the CA flag set? (y/n)?: n

kiran@ip-172-31-30-41:/data1/Kiran/SEC_YOCTO/cst-4.0.0/crts$ ../linux64/bin/srktool -a -d sha256 -s sha384 -t SRK_1_2_3_4_table.bin -e SRK_1_2_3_4_fuse.bin -f 1 -c ./SRK1_sha384_secp384r1_v3_usr_crt.pem,./SRK2_sha384_secp384r1_v3_usr_crt.pem,./SRK3_sha384_secp384r1_v3_usr_crt.pem,./SRK4_sha384_secp384r1_v3_usr_crt.pem

Number of certificates    = 4

SRK table binary filename = SRK_1_2_3_4_table.bin

SRK Fuse binary filename  = SRK_1_2_3_4_fuse.bin

SRK Fuse binary dump:

SRKH[0] = 0x6B8C7EE0

SRKH[1] = 0x18EF2C9C

SRKH[2] = 0xF08294BB

SRKH[3] = 0x0F81D4E7

SRKH[4] = 0xFBF5ECC7

SRKH[5] = 0xD1604A8F

SRKH[6] = 0xB026FF45

SRKH[7] = 0xF1B499F4

 

kiran@ip-172-31-30-41:/data1/Kiran/SEC_YOCTO/cst-4.0.0/crts$ openssl dgst -binary -sha256 SRK_1_2_3_4_table.bin

?~?k?,??????ԁ?????J`?E?&?????kiran@ip-172-31-30-41:/data1/Kiran/SEC_YOCTO/cst-4.0.0/crts$ od -t x4 --endian=big SRK_1_2_3_4_fuse.bin

0000000 e07e8c6b 9c2cef18 bb9482f0 e7d4810f

0000020 c7ecf5fb 8f4a60d1 45ff26b0 f499b4f1

0000040

kiran@ip-172-31-30-41:/data1/Kiran/SEC_YOCTO/cst-4.0.0/crts$ sha256sum SRK_1_2_3_4_table.bin

e07e8c6b9c2cef18bb9482f0e7d4810fc7ecf5fb8f4a60d145ff26b0f499b4f1  SRK_1_2_3_4_table.bin

 

Can you please guide me on which fuse addresses do I have to flash the below?:

SRK Fuse binary dump:

SRKH[0] = 0x6B8C7EE0

SRKH[1] = 0x18EF2C9C

SRKH[2] = 0xF08294BB

SRKH[3] = 0x0F81D4E7

SRKH[4] = 0xFBF5ECC7

SRKH[5] = 0xD1604A8F

SRKH[6] = 0xB026FF45

SRKH[7] = 0xF1B499F4

Also, any other steps that I need to do after flashing the keys?

Thx,

Kiran.

0 项奖励
回复

2,742 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Please raise a Confidential assistance ticket for fuse information support.

 

Regards

Harvey

 

 

0 项奖励
回复

3,211 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

secure boot isn't supported for FRDM board.

 

Regards

Harvey

0 项奖励
回复